1968422_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1968422_en-US

1968422_en-US

88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"

hi,

I am using imx8mp with 88w8997 wifi/BT AW-CM276 module for wifi connectivity and bluetooth. we are loadin the firmware "sdsd8997_combo_v4.bin" to the wifi/bt module. after the wifi connection is on going an error is occuring which is find from the dmesg. can you please help me with this?


error log

********************************


10-08 04:37:47.070 4108 4108 W CMD_RESP: cmd 0x256 error, result=0x2 wlan_process_cmdresp_error
10-08 04:37:47.078 4108 4108 E IOCTL failed: 00000000fe461547 id=0x50000, sub_id=0x50009 action=2, status_code=0x3
10-08 04:37:47.087 363 363 E : get link layer statistic fail
10-08 04:37:46.920 571 682 E WifiVendorHal: getWifiLinkLayerStats_1_6_Internal(l.1199) failed {.code = ERROR_UNKNOWN, .description = unknown}

Re: 88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"

hi @shaun_wu 

we have added the mbtchar driver from the Android 11 , and done some modification in the Bluetooth HAL , right now the we are able to up and run the bluetooth in our device with same "sdsd8997_combo_v4.bin" .


Thank you

Re: 88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"

hello @jeevanefx123 


for driver download:

git clone http://source.codeaurora.org/external/imx/mwifiex


Best Regards

Shaun

Re: 88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"

HI @shaun_wu 

can you please mention the driver for the same.?

Re: 88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"

Hello @jeevanefx123 


Please try following firmware: imx-firmware/nxp/FwImage_8997_SD/sdiouart8997_combo_v4.bin at lf-5.15.71_2.2.0 · nxp-imx/imx-firmwar...



Best Regards

Shaun

Re: 88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"

hi @shaun_wu ,

I have loaded this firmware , and i am able to connect both bluetooth and wifi simultaneously. ANd it is working fine.  So you are saying that the above issue is related to using the sdsd8997_combo_v4.bin firmware right?


Re: 88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"

Hello @jeevanefx123 


"sdsd8997_combo_v4.bin" this firmware is for sd-bt. AW-CM276 is not support BT with SD interface. Your Wi-Fi is SD interface, so Wi-Fi no problem. If you run BT, there will be problem.


Best Regards

Shaun

Re: 88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"

hi @shaun_wu ,

This is the log of Wifi and bt driver loading

01-01 00:00:07.276 178 178 F wlan : Loading MWLAN driver
01-01 00:00:07.281 178 178 F wlan : Register to Bus Driver...
01-01 00:00:07.286 178 178 F wlan : Register to SDIO_MMC Bus Driver
01-01 00:00:07.292 178 178 F : vendor=0x02DF device=0x9141 class=0 function=1
01-01 00:00:07.298 178 178 F : Attach moal handle ops, card interface type: 0x104
01-01 00:00:07.305 178 178 F : rps set to 0 from module param
01-01 00:00:07.311 178 178 F SD8997 : init module param from usr cfg
01-01 00:00:07.317 178 178 F card_type: SD8997, config block: 0
01-01 00:00:07.322 178 178 F : cfg80211_wext=0xf
01-01 00:00:07.326 178 178 F : sta_name=wlan
01-01 00:00:07.329 178 178 F : uap_name=wlan
01-01 00:00:07.332 178 178 F : wfd_name=p2p
01-01 00:00:07.336 178 178 F : max_vir_bss=1
01-01 00:00:07.339 178 178 F : cal_data_cfg=none
01-01 00:00:07.342 178 178 F : ps_mode = 1
01-01 00:00:07.346 178 178 F : auto_ds = 1
01-01 00:00:07.349 178 178 F : host_mlme=enable
01-01 00:00:07.352 178 178 F : fw_name=nxp/sdsd8997_combo_v4.bin
01-01 00:00:07.358 178 178 F SDIO : max_segs=128 max_seg_size=65535
01-01 00:00:07.363 178 178 F : rx_work=1 cpu_num=4
01-01 00:00:07.367 178 178 W : Attach mlan adapter operations.card_type is 0x104.
01-01 00:00:07.379 178 178 W wlan : Enable TX SG mode
01-01 00:00:07.383 178 178 W wlan : Enable RX SG mode
01-01 00:00:07.394 178 178 F Request firmware: nxp/sdsd8997_combo_v4.bin
01-01 00:00:07.415 178 178 W : mlan_dnld_fw
01-01 00:00:07.423 178 178 W : Check if firmware is already running
01-01 00:00:07.429 178 178 W wlan_sdio_check_fw_status: Wait for firmware initialization event
01-01 00:00:07.486 1 1 E pstore : crypto_comp_decompress failed, ret = -22!
01-01 00:00:07.503 1 1 I : Registered swp emulation handler
01-01 00:00:07.610 186 186 I logd.auditd: start
01-01 00:00:07.613 193 193 I watchdogd: watchdogd started (interval 10, margin 20)!
01-01 00:00:07.644 186 186 I logd : Loaded bug_map file: /vendor/etc/selinux/selinux_denial_metadata
01-01 00:00:07.653 186 186 I logd : Loaded bug_map file: /system/etc/selinux/bug_map
01-01 00:00:07.809 1 1 I zram0 : detected capacity change from 0 to 1228800
01-01 00:00:07.842 1 1 I mkswap : Swapspace size: 614396k, UUID=610c7397-03f1-42a0-926f-30c0925d3fad
01-01 00:00:07.872 1 1 I : Adding 614396k swap on /dev/block/zram0. Priority:-2 extents:1 across:614396k SS
01-01 00:00:08.033 224 224 D vdc : Waited 0ms for vold
01-01 00:00:08.086 233 233 D vdc : Waited 0ms for vold
01-01 00:00:08.217 201 201 I fsck.f2fs: Info: Fix the reported corruption.
01-01 00:00:08.223 201 201 I fsck.f2fs: Info: not exist /proc/version!
01-01 00:00:08.229 201 201 I fsck.f2fs: Info: Segments per section = 1
01-01 00:00:08.235 201 201 I fsck.f2fs: Info: Sections per zone = 1
01-01 00:00:08.240 201 201 I fsck.f2fs: Info: sector size = 4096
01-01 00:00:08.246 201 201 I fsck.f2fs: Info: total sectors = 6197760 (24210 MB)
01-01 00:00:08.252 201 201 I fsck.f2fs: Info: MKFS version
01-01 00:00:08.257 201 201 I fsck.f2fs: "5.15.74-gd14ab594eb48-dirty"
01-01 00:00:08.263 201 201 I fsck.f2fs: Info: FSCK version
01-01 00:00:08.268 201 201 I fsck.f2fs: from "5.15.74-gd14ab594eb48-dirty"
01-01 00:00:08.358 201 201 I F2FS-fs (dm-38): Using encoding defined by superblock: utf8-12.1.0 with flags 0x0
01-01 00:00:08.453 201 201 I F2FS-fs (dm-38): recover_inode: ino = 317d, name = , inline = 21
01-01 00:00:08.462 201 201 I F2FS-fs (dm-38): recover_data: ino = 317d (i_size: recover) recovered = 1, err = 0
01-01 00:00:08.472 201 201 I F2FS-fs (dm-38): recover_inode: ino = 1d1a, name = , inline = 21
01-01 00:00:08.480 201 201 I F2FS-fs (dm-38): recover_data: ino = 1d1a (i_size: recover) recovered = 0, err = 0
01-01 00:00:08.490 201 201 I F2FS-fs (dm-38): recover_inode: ino = 317e, name = , inline = 21
01-01 00:00:08.499 201 201 I F2FS-fs (dm-38): recover_dentry: ino = 317e, name = , dir = 177a, err = 0
01-01 00:00:08.509 201 201 I F2FS-fs (dm-38): recover_data: ino = 317e (i_size: recover) recovered = 1, err = 0
01-01 00:00:08.518 201 201 I F2FS-fs (dm-38): recover_inode: ino = 3177, name = , inline = 21
01-01 00:00:08.527 201 201 I F2FS-fs (dm-38): recover_data: ino = 3177 (i_size: recover) recovered = 1, err = 0
01-01 00:00:08.536 201 201 I F2FS-fs (dm-38): recover_inode: ino = 1d1a, name = , inline = 21
01-01 00:00:08.545 201 201 I F2FS-fs (dm-38): recover_data: ino = 1d1a (i_size: recover) recovered = 1, err = 0
01-01 00:00:08.561 201 201 I F2FS-fs (dm-38): checkpoint: version = 276aec00
01-01 00:00:08.568 201 201 I F2FS-fs (dm-38): Mounted with checkpoint version = 276aec00
01-01 00:00:08.569 178 178 W Wlan : FW download over, firmwarelen=623240 downloaded 623240
01-01 00:00:08.582 178 178 W wlan_sdio_check_fw_status: Wait for firmware initialization event
01-01 00:00:08.647 259 259 D vdc : Waited 0ms for vold
01-01 00:00:08.673 1 1 I fscrypt : AES-256-CTS-CBC using implementation "cts-cbc-aes-ce"
01-01 00:00:08.776 201 201 E vold : keystore2 Keystore earlyBootEnded returned service specific error: -68
01-01 00:00:08.836 199 199 I logd : logd reinit
01-01 00:00:08.843 199 199 E logd : FrameworkListener: read() failed (Connection reset by peer)
01-01 00:00:08.843 268 268 I apexd : Scanning /system/apex for pre-installed ApexFiles
01-01 00:00:08.859 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.adbd.capex
01-01 00:00:08.867 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.adservices.capex
01-01 00:00:08.877 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.apex.cts.shim.apex
01-01 00:00:08.886 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.appsearch.apex
01-01 00:00:08.895 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.art.capex
01-01 00:00:08.904 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.btservices.apex
01-01 00:00:08.913 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.car.framework.apex
01-01 00:00:08.922 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.cellbroadcast.capex
01-01 00:00:08.931 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.conscrypt.capex
01-01 00:00:09.069 270 270 I loop4 : detected capacity change from 0 to 41784
01-01 00:00:09.077 271 271 I loop5 : detected capacity change from 0 to 6952
01-01 00:00:09.139 270 270 I EXT4-fs (loop4): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.140 271 271 I EXT4-fs (loop5): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.152 270 270 I loop6 : detected capacity change from 0 to 12952
01-01 00:00:09.165 271 271 I loop7 : detected capacity change from 0 to 536
01-01 00:00:09.219 270 270 I EXT4-fs (loop6): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.234 270 270 I loop8 : detected capacity change from 0 to 1728
01-01 00:00:09.237 271 271 I EXT4-fs (loop7): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.254 271 271 I loop9 : detected capacity change from 0 to 536
01-01 00:00:09.296 270 270 I EXT4-fs (loop8): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.307 270 270 I loop10 : detected capacity change from 0 to 74600
01-01 00:00:09.341 271 271 I EXT4-fs (loop9): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.352 271 271 I loop11 : detected capacity change from 0 to 96704
01-01 00:00:09.371 270 270 I EXT4-fs (loop10): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.383 270 270 I loop12 : detected capacity change from 0 to 3920
01-01 00:00:09.411 271 271 I EXT4-fs (loop11): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.420 178 178 F : WLAN FW is active
01-01 00:00:09.422 271 271 I loop13 : detected capacity change from 0 to 16240
01-01 00:00:09.425 178 178 F : on_time is 9252720625
01-01 00:00:09.442 270 270 I EXT4-fs (loop12): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.454 270 270 I loop14 : detected capacity change from 0 to 536
01-01 00:00:09.476 66 66 W : fw_cap_info=0x18fcffa3, dev_cap_mask=0xffffffff
01-01 00:00:09.483 66 66 W : max_p2p_conn = 8, max_sta_conn = 8
01-01 00:00:09.500 178 178 F : Register NXP 802.11 Adapter wlan0
01-01 00:00:09.506 178 178 F wlan : wlan%d set max_mtu 2000
01-01 00:00:09.511 271 271 I EXT4-fs (loop13): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.512 178 178 F : Register NXP 802.11 Adapter wlan1
01-01 00:00:09.522 271 271 I loop15 : detected capacity change from 0 to 1536
01-01 00:00:09.523 270 270 I EXT4-fs (loop14): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.531 178 178 F : Register NXP 802.11 Adapter p2p0
01-01 00:00:09.533 270 270 I loop16 : detected capacity change from 0 to 17256
01-01 00:00:09.542 178 178 F wlan : version = SD8997----16.68.1.p197-MM5X16368.p2-GPL-(FP92)
01-01 00:00:09.562 178 178 E WLAN : SDIO Driver Registration SUCCESS
01-01 00:00:09.568 178 178 F wlan : Register to Bus Driver Done
01-01 00:00:09.573 178 178 F wlan : Driver loaded successfully
01-01 00:00:09.584 178 178 F BT : Loading driver
01-01 00:00:09.597 178 178 F : BT FW is active(0)
01-01 00:00:09.601 270 270 I device-mapper: verity: sha256 using implementation "sha256-ce"
01-01 00:00:09.601 178 178 F BT : FW already downloaded!
01-01 00:00:09.619 271 271 I EXT4-fs (loop15): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.630 271 271 I loop17 : detected capacity change from 0 to 40512
01-01 00:00:09.630 178 178 F BT : Create /dev/mbtchar0
01-01 00:00:09.640 270 270 I EXT4-fs (dm-36): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.653 270 270 I loop18 : detected capacity change from 0 to 17128
01-01 00:00:09.677 271 271 I device-mapper: verity: sha256 using implementation "sha256-ce"
01-01 00:00:09.705 178 178 F BT : Create /dev/mdebugchar0
01-01 00:00:09.709 270 270 I device-mapper: verity: sha256 using implementation "sha256-ce"
01-01 00:00:09.728 271 271 I EXT4-fs (dm-35): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.732 270 270 I EXT4-fs (dm-34): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.734 270 270 I loop19 : detected capacity change from 0 to 29504
01-01 00:00:09.744 178 178 F BT : Driver loaded successfully

Re: 88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"

hi @shaun_wu ,

From the below logs you can see both bluetooth and wifi drivers are up and running.



--------- beginning of kernel
01-01 00:00:00.000 0 0 I : Booting Linux on physical CPU 0x0000000000 [0x410fd034]
01-01 00:00:00.000 0 0 I : Linux version 5.15.74-gd14ab594eb48-dirty (jeevan@EFXSEZPC024) (Android (8508608, based on r450784e) clang version 14.0.7 (https://android.googlesource.com/toolchain/llvm-project 4c603efb0cca074e9238af8b4106c30add4418f6), LLD 14.0.7) #22 SMP PREEMPT Fri Sep 27 21:46:43 IST 2024
01-01 00:00:00.000 0 0 I Machine model: ADLINK LEC-iMX8MP SOM module
01-01 00:00:00.000 0 0 I : Stack Depot is disabled
01-01 00:00:00.000 0 0 I earlycon: ec_imx6q0 at MMIO 0x0000000030890000 (options '115200')
01-01 00:00:00.000 0 0 I printk : bootconsole [ec_imx6q0] enabled
01-01 00:00:00.000 0 0 I efi : UEFI not found.
01-01 00:00:00.000 0 0 I Reserved memory: created DMA memory pool at 0x0000000094300000, size 1 MiB
01-01 00:00:00.000 0 0 I OF : reserved mem: initialized node vdev0buffer@94300000, compatible id shared-dma-pool
01-01 00:00:00.000 0 0 I kvm [0] : Reserved 16 MiB at 0xbec00000
01-01 00:00:00.000 0 0 I Zone ranges:
01-01 00:00:00.000 0 0 I : DMA32 [mem 0x0000000040000000-0x00000000bfffffff]
01-01 00:00:00.000 0 0 I : Normal empty
01-01 00:00:00.000 0 0 I : Movable zone start for each node
01-01 00:00:00.000 0 0 I : Early memory node ranges
01-01 00:00:00.000 0 0 I node 0: [mem 0x0000000040000000-0x00000000557fffff]
01-01 00:00:00.000 0 0 I node 0: [mem 0x0000000055800000-0x0000000055ffffff]
01-01 00:00:00.000 0 0 I node 0: [mem 0x0000000056000000-0x00000000823fffff]
01-01 00:00:00.000 0 0 I node 0: [mem 0x0000000082400000-0x00000000943fffff]
01-01 00:00:00.000 0 0 I node 0: [mem 0x0000000094400000-0x00000000bfffffff]
01-01 00:00:00.000 0 0 I : Initmem setup node 0 [mem 0x0000000040000000-0x00000000bfffffff]
01-01 00:00:00.000 0 0 I cma : Reserved 400 MiB at 0x000000009f000000
01-01 00:00:00.000 0 0 I psci : probing for conduit method from DT.
01-01 00:00:00.000 0 0 I psci : PSCIv1.1 detected in firmware.
01-01 00:00:00.000 0 0 I psci : Using standard PSCI v0.2 function IDs
01-01 00:00:00.000 0 0 I psci : MIGRATE_INFO_TYPE not supported.
01-01 00:00:00.000 0 0 I psci : SMC Calling Convention v1.2
01-01 00:00:00.000 0 0 I Load bootconfig: 1030 bytes 65 nodes
01-01 00:00:00.000 0 0 I percpu : Embedded 29 pages/cpu s81816 r8192 d28776 u118784
01-01 00:00:00.000 0 0 D pcpu-alloc: s81816 r8192 d28776 u118784 alloc=29*4096
01-01 00:00:00.000 0 0 D pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
01-01 00:00:00.000 0 0 I : Detected VIPT I-cache on CPU0
01-01 00:00:00.000 0 0 W CPU features: SYS_ID_AA64MMFR1_EL1[11:8]: already set to 0
01-01 00:00:00.000 0 0 I CPU features: detected: GIC system register CPU interface
01-01 00:00:00.000 0 0 I CPU features: detected: ARM erratum 845719
01-01 00:00:00.000 0 0 I : Built 1 zonelists, mobility grouping on. Total pages: 516096
01-01 00:00:00.000 0 0 I : Kernel command line: stack_depot_disable=on kasan.stacktrace=off kvm-arm.mode=protected cgroup_disable=pressure console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 init=/init firmware_class.path=/vendor/firmware loop.max_part=7 bootconfig transparent_hugepage=never swiotlb=65536 androidboot.selinux=permissive moal.mod_para=wifi_mod_para.conf pci=nomsi cma=400M@0x400M-0xb80M galcore.contiguousSize=33554432 bootconfig buildvariant=userdebug
01-01 00:00:00.000 0 0 I cgroup : Disabling pressure control group feature
01-01 00:00:00.000 0 0 I : Unknown kernel command line parameters "buildvariant=userdebug", will be passed to user space.
01-01 00:00:00.000 0 0 I : Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
01-01 00:00:00.000 0 0 I : Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
01-01 00:00:00.000 0 0 I mem auto-init: stack:all(zero), heap alloc:on, heap free:off
01-01 00:00:00.000 0 0 I Memory : 1262660K/2097152K available (18112K kernel code, 2238K rwdata, 18812K rodata, 1408K init, 604K bss, 424892K reserved, 409600K cma-reserved)
01-01 00:00:00.000 0 0 I SLUB : HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
01-01 00:00:00.000 0 0 I : trace event string verifier disabled
01-01 00:00:00.000 0 0 I rcu : Preemptible hierarchical RCU implementation.
01-01 00:00:00.000 0 0 I rcu : RCU event tracing is enabled.
01-01 00:00:00.000 0 0 I rcu : RCU dyntick-idle grace-period acceleration is enabled.
01-01 00:00:00.000 0 0 I rcu : RCU restricting CPUs from NR_CPUS=32 to nr_cpu_ids=4.
01-01 00:00:00.000 0 0 I rcu : RCU priority boosting: priority 1 delay 500 ms.
01-01 00:00:00.000 0 0 I : Trampoline variant of Tasks RCU enabled.
01-01 00:00:00.000 0 0 I : Tracing variant of Tasks RCU enabled.
01-01 00:00:00.000 0 0 I rcu : RCU calculated value of scheduler-enlistment delay is 25 jiffies.
01-01 00:00:00.000 0 0 I rcu : Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
01-01 00:00:00.000 0 0 I NR_IRQS : 64, nr_irqs: 64, preallocated irqs: 0
01-01 00:00:00.000 0 0 I GICv3 : GIC: Using split EOI/Deactivate mode
01-01 00:00:00.000 0 0 I GICv3 : 160 SPIs implemented
01-01 00:00:00.000 0 0 I GICv3 : 0 Extended SPIs implemented
01-01 00:00:00.000 0 0 I GICv3 : Distributor has no Range Selector support
01-01 00:00:00.000 0 0 I : Root IRQ handler: gic_handle_irq.10d7cf410c142aff6d31b6303c3f9f87.cfi_jt
01-01 00:00:00.000 0 0 I GICv3 : 16 PPIs implemented
01-01 00:00:00.000 0 0 I GICv3 : CPU0: found redistributor 0 region 0:0x0000000038880000
01-01 00:00:00.000 0 0 W ITS : No ITS available, not enabling LPIs
01-01 00:00:00.000 0 0 I rcu : Offload RCU callbacks from CPUs: (none).
01-01 00:00:00.000 0 0 I kfence : initialized - using 524288 bytes for 63 objects at 0x(____ptrval____)-0x(____ptrval____)
01-01 00:00:00.000 0 0 I arch_timer: cp15 timer(s) running at 8.00MHz (phys).
01-01 00:00:00.000 0 0 I clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
01-01 00:00:00.000 0 0 I sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
01-01 00:00:00.009 0 0 I : Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
01-01 00:00:00.019 0 0 I pid_max : default: 32768 minimum: 301
01-01 00:00:00.025 0 0 I LSM : Security Framework initializing
01-01 00:00:00.030 0 0 I SELinux : Initializing.
01-01 00:00:00.034 0 0 I : Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
01-01 00:00:00.042 0 0 I : Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
01-01 00:00:00.053 1 1 I rcu : Hierarchical SRCU implementation.
01-01 00:00:00.057 1 1 I dyndbg : Ignore empty _ddebug table in a CONFIG_DYNAMIC_DEBUG_CORE build
01-01 00:00:00.065 1 1 I : EFI services will not be available.
01-01 00:00:00.070 1 1 I smp : Bringing up secondary CPUs ...
01-01 00:00:00.076 0 0 I : Detected VIPT I-cache on CPU1
01-01 00:00:00.076 0 0 I GICv3 : CPU1: found redistributor 1 region 0:0x00000000388a0000
01-01 00:00:00.076 0 0 I CPU1 : Booted secondary processor 0x0000000001 [0x410fd034]
01-01 00:00:00.077 0 0 I : Detected VIPT I-cache on CPU2
01-01 00:00:00.077 0 0 I GICv3 : CPU2: found redistributor 2 region 0:0x00000000388c0000
01-01 00:00:00.077 0 0 I CPU2 : Booted secondary processor 0x0000000002 [0x410fd034]
01-01 00:00:00.078 0 0 I : Detected VIPT I-cache on CPU3
01-01 00:00:00.078 0 0 I GICv3 : CPU3: found redistributor 3 region 0:0x00000000388e0000
01-01 00:00:00.078 0 0 I CPU3 : Booted secondary processor 0x0000000003 [0x410fd034]
01-01 00:00:00.078 1 1 I smp : Brought up 1 node, 4 CPUs
01-01 00:00:00.139 1 1 I SMP : Total of 4 processors activated.
01-01 00:00:00.144 1 1 I CPU features: detected: 32-bit EL0 Support
01-01 00:00:00.150 1 1 I CPU features: detected: 32-bit EL1 Support
01-01 00:00:00.156 1 1 I CPU features: detected: CRC32 instructions
01-01 00:00:00.162 1 1 I CPU features: detected: Protected KVM
01-01 00:00:00.167 1 1 I CPU features: emulated: Privileged Access Never (PAN) using TTBR0_EL1 switching
01-01 00:00:00.187 1 1 I : CPU: All CPU(s) started at EL2
01-01 00:00:00.189 19 19 I alternatives: patching kernel code
01-01 00:00:00.210 1 1 I : Registered cp15_barrier emulation handler
01-01 00:00:00.213 1 1 I : Registered setend emulation handler
01-01 00:00:00.218 1 1 W : KASLR disabled due to lack of seed
01-01 00:00:00.223 1 1 I clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
01-01 00:00:00.234 1 1 I : futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
01-01 00:00:00.254 1 1 I pinctrl core: initialized pinctrl subsystem
01-01 00:00:00.259 1 1 I NET : Registered PF_NETLINK/PF_ROUTE protocol family
01-01 00:00:00.266 1 1 I DMA : preallocated 256 KiB GFP_KERNEL pool for atomic allocations
01-01 00:00:00.272 1 1 I DMA : preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
01-01 00:00:00.280 1 1 I audit : initializing netlink subsys (disabled)
01-01 00:00:00.287 1 1 I thermal_sys: Registered thermal governor 'step_wise'
01-01 00:00:00.295 1 1 I thermal_sys: Registered thermal governor 'user_space'
01-01 00:00:00.302 1 1 I thermal_sys: Registered thermal governor 'power_allocator'
01-01 00:00:00.309 1 1 I cpuidle : using governor menu
01-01 00:00:00.321 1 1 I hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
01-01 00:00:00.328 1 1 I : ASID allocator initialised with 65536 entries
01-01 00:00:00.334 1 1 I Serial : AMBA PL011 UART driver
01-01 00:00:00.339 1 1 I : imx rpmsg driver is registered.
01-01 00:00:00.348 1 1 I printk : console [ramoops-1] enabled
01-01 00:00:00.351 1 1 I pstore : Registered ramoops as persistent store backend
01-01 00:00:00.358 1 1 I ramoops : using 0x100000@0x94400000, ecc: 0
01-01 00:00:00.397 1 1 I platform 32fd8000.hdmi: Fixing up cyclic dependency with 32fc6000.lcd-controller
01-01 00:00:00.425 1 1 I iommu : Default domain type: Translated
01-01 00:00:00.427 1 1 I iommu : DMA domain TLB invalidation policy: strict mode
01-01 00:00:00.435 1 1 I : SCSI subsystem initialized
01-01 00:00:00.439 1 1 I usbcore : registered new interface driver usbfs
01-01 00:00:00.445 1 1 I usbcore : registered new interface driver hub
01-01 00:00:00.451 1 1 I usbcore : registered new device driver usb
01-01 00:00:00.457 1 1 I mc : Linux media interface: v0.10
01-01 00:00:00.462 1 1 I videodev: Linux video capture interface: v2.00
01-01 00:00:00.468 1 1 I pps_core: LinuxPPS API ver. 1 registered
01-01 00:00:00.474 1 1 I pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti
01-01 00:00:00.484 1 1 I : PTP clock support registered
01-01 00:00:00.488 1 1 I EDAC MC : Ver: 3.0.0
01-01 00:00:00.493 1 1 I : FPGA manager framework
01-01 00:00:00.496 1 1 I : Advanced Linux Sound Architecture Driver Initialized.
01-01 00:00:00.504 1 1 I Bluetooth: Core ver 2.22
01-01 00:00:00.507 1 1 I NET : Registered PF_BLUETOOTH protocol family
01-01 00:00:00.513 1 1 I Bluetooth: HCI device and connection manager initialized
01-01 00:00:00.520 1 1 I Bluetooth: HCI socket layer initialized
01-01 00:00:00.526 1 1 I Bluetooth: L2CAP socket layer initialized
01-01 00:00:00.532 1 1 I Bluetooth: SCO socket layer initialized
01-01 00:00:00.538 1 1 I nfc : nfc_init: NFC Core ver 0.1
01-01 00:00:00.542 1 1 I NET : Registered PF_NFC protocol family
01-01 00:00:00.548 1 1 I clocksource: Switched to clocksource arch_sys_counter
01-01 00:00:00.607 1 1 I VFS : Disk quotas dquot_6.6.0
01-01 00:00:00.609 1 1 I VFS : Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
01-01 00:00:00.617 1 1 I NET : Registered PF_INET protocol family
01-01 00:00:00.622 1 1 I : IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
01-01 00:00:00.631 1 1 I : tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
01-01 00:00:00.639 1 1 I : Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
01-01 00:00:00.648 1 1 I : TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
01-01 00:00:00.656 1 1 I : TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
01-01 00:00:00.665 1 1 I TCP : Hash tables configured (established 16384 bind 16384)
01-01 00:00:00.672 1 1 I : UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
01-01 00:00:00.679 1 1 I : UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
01-01 00:00:00.687 1 1 I NET : Registered PF_UNIX/PF_LOCAL protocol family
01-01 00:00:00.693 1 1 I NET : Registered PF_XDP protocol family
01-01 00:00:00.699 1 1 I PCI : CLS 0 bytes, default 64
01-01 00:00:00.704 8 8 I : Trying to unpack rootfs image as initramfs...
01-01 00:00:00.710 1 1 I hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
01-01 00:00:00.720 1 1 I kvm [1] : IPA Size Limit: 40 bits
01-01 00:00:00.739 1 1 I kvm [1] : GICv3: no GICV resource entry
01-01 00:00:00.742 1 1 I kvm [1] : disabling GICv2 emulation
01-01 00:00:00.747 1 1 I kvm [1] : GIC system register CPU interface enabled
01-01 00:00:00.754 1 1 I kvm [1] : vgic interrupt IRQ9
01-01 00:00:00.758 1 1 I kvm [1] : Protected nVHE mode initialized successfully
01-01 00:00:00.767 1 1 I : Initialise system trusted keyrings
01-01 00:00:00.771 1 1 I workingset: timestamp_bits=46 max_order=19 bucket_order=0
01-01 00:00:00.788 1 1 I fuse : init (API version 7.36)
01-01 00:00:00.831 1 1 I : Key type asymmetric registered
01-01 00:00:00.833 1 1 I : Asymmetric key parser 'x509' registered
01-01 00:00:00.839 1 1 I : Block layer SCSI generic (bsg) driver version 0.4 loaded (major 237)
01-01 00:00:00.847 1 1 I : io scheduler mq-deadline registered
01-01 00:00:00.852 1 1 I : io scheduler kyber registered
01-01 00:00:00.857 1 1 I : io scheduler bfq registered
01-01 00:00:00.879 1 1 I brd : module loaded
01-01 00:00:00.893 1 1 I loop : module loaded
01-01 00:00:00.897 1 1 I wireguard: WireGuard 1.0.0 loaded. See www.wireguard.com for information.
01-01 00:00:00.903 1 1 I wireguard: Copyright (C) 2015-2019 Jason A. Donenfeld . All Rights Reserved.
01-01 00:00:00.914 1 1 I : MACsec IEEE 802.1AE
01-01 00:00:00.918 1 1 I tun : Universal TUN/TAP device driver, 1.6
01-01 00:00:00.923 1 1 I : PPP generic driver version 2.4.2
01-01 00:00:00.928 1 1 I : PPP BSD Compression module registered
01-01 00:00:00.933 1 1 I : PPP Deflate Compression module registered
01-01 00:00:00.939 1 1 I : PPP MPPE Compression module registered
01-01 00:00:00.945 1 1 I NET : Registered PF_PPPOX protocol family
01-01 00:00:00.950 1 1 I : PPTP driver version 0.8.5
01-01 00:00:00.955 1 1 I usbcore : registered new interface driver rtl8150
01-01 00:00:00.961 1 1 I usbcore : registered new interface driver r8152
01-01 00:00:00.967 1 1 I usbcore : registered new interface driver asix
01-01 00:00:00.974 1 1 I usbcore : registered new interface driver ax88179_178a
01-01 00:00:00.980 1 1 I usbcore : registered new interface driver cdc_ether
01-01 00:00:00.987 1 1 I usbcore : registered new interface driver cdc_eem
01-01 00:00:00.989 8 8 I : Freeing initrd memory: 22260K
01-01 00:00:00.993 1 1 I usbcore : registered new interface driver cdc_ncm
01-01 00:00:01.004 1 1 I usbcore : registered new interface driver aqc111
01-01 00:00:01.011 1 1 I usbcore : registered new interface driver r8153_ecm
01-01 00:00:01.019 1 1 I ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
01-01 00:00:01.024 1 1 I ehci-pci: EHCI PCI platform driver
01-01 00:00:01.030 1 1 I ehci-platform: EHCI generic platform driver
01-01 00:00:01.036 1 1 I usbcore : registered new interface driver cdc_acm
01-01 00:00:01.042 1 1 I cdc_acm : USB Abstract Control Model driver for USB modems and ISDN adapters
01-01 00:00:01.051 1 1 I usbcore : registered new interface driver uas
01-01 00:00:01.057 1 1 I usbcore : registered new interface driver usb-storage
01-01 00:00:01.064 1 1 I usbcore : registered new interface driver xpad
01-01 00:00:01.070 1 1 I usbcore : registered new interface driver uvcvideo
01-01 00:00:01.076 1 1 I gspca_main: v2.14.0 registered
01-01 00:00:01.081 1 1 I device-mapper: uevent: version 1.0.3
01-01 00:00:01.086 1 1 I device-mapper: ioctl: 4.45.0-ioctl (2021-03-22) initialised: [email protected]
01-01 00:00:01.096 1 1 I Bluetooth: HCI UART driver ver 2.3
01-01 00:00:01.101 1 1 I Bluetooth: HCI UART protocol H4 registered
01-01 00:00:01.106 1 1 I Bluetooth: HCI UART protocol LL registered
01-01 00:00:01.112 1 1 I Bluetooth: HCI UART protocol Broadcom registered
01-01 00:00:01.119 1 1 I Bluetooth: HCI UART protocol QCA registered
01-01 00:00:01.125 1 1 I sdhci : Secure Digital Host Controller Interface driver
01-01 00:00:01.132 1 1 I sdhci : Copyright(c) Pierre Ossman
01-01 00:00:01.137 1 1 I sdhci-pltfm: SDHCI platform and OF driver helper
01-01 00:00:01.143 1 1 I SMCCC : SOC_ID: ARCH_SOC_ID not implemented, skipping ....
01-01 00:00:01.150 1 1 I hid : raw HID events driver (C) Jiri Kosina
01-01 00:00:01.157 1 1 I usbcore : registered new interface driver usbhid
01-01 00:00:01.162 1 1 I usbhid : USB HID core driver
01-01 00:00:01.167 1 1 I ashmem : initialized
01-01 00:00:01.171 1 1 I gnss : GNSS driver registered with major 507
01-01 00:00:01.177 1 1 I usbcore : registered new interface driver snd-usb-audio
01-01 00:00:01.184 1 1 I : GACT probability NOT on
01-01 00:00:01.188 1 1 I : Mirror/redirect action on
01-01 00:00:01.192 1 1 I netem : version 1.3
01-01 00:00:01.196 1 1 I : u32 classifier
01-01 00:00:01.199 1 1 I : input device check on
01-01 00:00:01.204 1 1 I : Actions configured
01-01 00:00:01.209 1 1 I xt_time : kernel timezone is -0000
01-01 00:00:01.213 1 1 I ipip : IPv4 and MPLS over IPv4 tunneling driver
01-01 00:00:01.220 1 1 I gre : GRE over IPv4 demultiplexor driver
01-01 00:00:01.225 1 1 I ip_gre : GRE over IPv4 tunneling driver
01-01 00:00:01.231 1 1 I : IPv4 over IPsec tunneling driver
01-01 00:00:01.236 1 1 I : Initializing XFRM netlink socket
01-01 00:00:01.240 1 1 I : IPsec XFRM device driver
01-01 00:00:01.245 1 1 I NET : Registered PF_INET6 protocol family
01-01 00:00:01.252 1 1 I : Segment Routing with IPv6
01-01 00:00:01.255 1 1 I : In-situ OAM (IOAM) with IPv6
01-01 00:00:01.259 1 1 I mip6 : Mobile IPv6
01-01 00:00:01.264 1 1 I sit : IPv6, IPv4 and MPLS over IPv4 tunneling driver
01-01 00:00:01.270 1 1 I ip6_gre : GRE over IPv6 tunneling driver
01-01 00:00:01.276 1 1 I NET : Registered PF_PACKET protocol family
01-01 00:00:01.281 1 1 I NET : Registered PF_KEY protocol family
01-01 00:00:01.287 1 1 I can : controller area network core
01-01 00:00:01.292 1 1 I NET : Registered PF_CAN protocol family
01-01 00:00:01.298 1 1 I Bluetooth: RFCOMM TTY layer initialized
01-01 00:00:01.303 1 1 I Bluetooth: RFCOMM socket layer initialized
01-01 00:00:01.308 1 1 I Bluetooth: RFCOMM ver 1.11
01-01 00:00:01.313 1 1 I Bluetooth: HIDP (Human Interface Emulation) ver 1.2
01-01 00:00:01.320 1 1 I Bluetooth: HIDP socket layer initialized
01-01 00:00:01.325 1 1 I l2tp_core: L2TP core driver, V2.0
01-01 00:00:01.330 1 1 I l2tp_ppp: PPPoL2TP kernel driver, V2.0
01-01 00:00:01.336 1 1 I 8021q : 802.1Q VLAN Support v1.8
01-01 00:00:01.341 1 1 I tipc : Activated (version 2.0.0)
01-01 00:00:01.346 1 1 I NET : Registered PF_TIPC protocol family
01-01 00:00:01.351 1 1 I tipc : Started in single node mode
01-01 00:00:01.357 1 1 I NET : Registered PF_IEEE802154 protocol family
01-01 00:00:01.363 1 1 I NET : Registered PF_VSOCK protocol family
01-01 00:00:01.369 1 1 I : registered taskstats version 1
01-01 00:00:01.373 1 1 I : Loading compiled-in X.509 certificates
01-01 00:00:01.380 65 65 I : cryptomgr_probe (65) used greatest stack depth: 14032 bytes left
01-01 00:00:01.382 1 1 I : Loaded X.509 cert 'Build time autogenerated kernel key: 1fc11d5d4d75c3373e5cabcd3a650022fc1458b5'
01-01 00:00:01.399 1 1 I : page_owner is disabled
01-01 00:00:01.401 1 1 I : Key type ._fscrypt registered
01-01 00:00:01.406 1 1 I : Key type .fscrypt registered
01-01 00:00:01.410 1 1 I : Key type fscrypt-provisioning registered
01-01 00:00:01.416 1 1 I pstore : Using crash dump compression: deflate
01-01 00:00:01.426 1 1 I : ALSA device list:
01-01 00:00:01.426 1 1 I : No soundcards found.
01-01 00:00:01.431 1 1 E : Warning: unable to open an initial console.
01-01 00:00:01.437 1 1 I : Freeing unused kernel memory: 1408K
01-01 00:00:01.469 1 1 I : Run /init as init process
01-01 00:00:01.470 1 1 D with arguments:
01-01 00:00:01.470 1 1 D : /init
01-01 00:00:01.470 1 1 D with environment:
01-01 00:00:01.470 1 1 D : HOME=/
01-01 00:00:01.470 1 1 D : TERM=linux
01-01 00:00:01.470 1 1 D : buildvariant=userdebug
01-01 00:00:01.474 1 1 I init : init first stage started!
01-01 00:00:01.477 1 1 E init : alias lines in modules.alias must have 3 entries, not 4
01-01 00:00:01.484 1 1 E init : alias lines in modules.alias must have 3 entries, not 4
01-01 00:00:01.493 1 1 E init : alias lines in modules.alias must have 3 entries, not 4
01-01 00:00:01.500 1 1 I init : Loading module /lib/modules/zsmalloc.ko with args ''
01-01 00:00:01.506 1 1 I zsmalloc: module verification failed: signature and/or required key missing - tainting kernel
01-01 00:00:01.518 1 1 I init : Loaded kernel module /lib/modules/zsmalloc.ko
01-01 00:00:01.523 1 1 I init : Loading module /lib/modules/zram.ko with args ''
01-01 00:00:01.532 1 1 I zram : Added device: zram0
01-01 00:00:01.534 1 1 I init : Loaded kernel module /lib/modules/zram.ko
01-01 00:00:01.540 1 1 I init : Loading module /lib/modules/soc-imx8m.ko with args ''
01-01 00:00:01.549 1 1 I SoC : i.MX8MP revision 1.1
01-01 00:00:01.552 1 1 I init : Loaded kernel module /lib/modules/soc-imx8m.ko
01-01 00:00:01.607 1 1 I : Bus freq driver module loaded
01-01 00:00:01.611 1 1 E : trusty trusty: failed to get version: -1
01-01 00:00:01.615 1 1 I : trusty trusty: selected api version: 0 (requested 5)
01-01 00:00:01.628 1 1 I imx8mp-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
01-01 00:00:01.645 1 1 I 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 37, base_baud = 1500000) is a IMX
01-01 00:00:01.645 1 1 I printk : console [ttymxc1] enabled
01-01 00:00:01.653 1 1 I printk : bootconsole [ec_imx6q0] disabled
01-01 00:00:01.670 1 1 I i2c-0 : IMX I2C adapter registered
01-01 00:00:01.676 1 1 I i2c-1 : IMX I2C adapter registered
01-01 00:00:01.683 1 1 I i2c 2-003c: Fixing up cyclic dependency with 32e40000.csi
01-01 00:00:01.690 1 1 I i2c-2 : IMX I2C adapter registered
01-01 00:00:01.713 1 1 I i2c-5 : IMX I2C adapter registered
01-01 00:00:01.720 1 1 I i2c_dev : i2c /dev entries driver
01-01 00:00:01.740 1 1 I nxp-pca9450 0-0025: pca9450bc probed.
01-01 00:00:01.750 1 1 W pwm-backlight lvds_backlight: supply power not found, using dummy regulator
01-01 00:00:01.769 8 8 I sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO
01-01 00:00:01.801 10 10 I mmc0 : SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
01-01 00:00:01.801 55 55 I mmc2 : SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
01-01 00:00:01.810 8 8 I mmc1 : SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
01-01 00:00:01.840 1 1 W imx8mq-usb-phy 381f0040.usb-phy: supply vbus not found, using dummy regulator
01-01 00:00:01.849 1 1 W imx8mq-usb-phy 382f0040.usb-phy: supply vbus not found, using dummy regulator
01-01 00:00:01.862 1 1 E snvs_pwrkey 30370000.snvs: snvs-powerkey: snvs pwkey: trusty driver failed to probe! nr=0xb5000000 error=-1. Use normal mode.
01-01 00:00:01.876 1 1 I input : 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
01-01 00:00:01.878 66 66 I mmc2 : new HS400 Enhanced strobe MMC card at address 0001
01-01 00:00:01.897 66 66 I mmcblk2 : mmc2:0001 IX2932 29.1 GiB
01-01 00:00:01.907 43 43 I mmc0 : new ultra high speed SDR104 SDIO card at address 0001
01-01 00:00:01.907 66 66 W : Alternate GPT is invalid, using primary GPT.
01-01 00:00:01.920 66 66 I mmcblk2 : p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15 p16
01-01 00:00:01.930 66 66 I mmcblk2boot0: mmc2:0001 IX2932 4.00 MiB
01-01 00:00:01.938 66 66 I mmcblk2boot1: mmc2:0001 IX2932 4.00 MiB
01-01 00:00:01.945 66 66 I mmcblk2rpmb: mmc2:0001 IX2932 4.00 MiB, chardev (511:0)
01-01 00:00:01.960 1 1 I dwhdmi-imx 32fd8000.hdmi: Detected HDMI TX controller v2.13a with HDCP (samsung_dw_hdmi_phy2)
01-01 00:00:01.972 1 1 I dwhdmi-imx 32fd8000.hdmi: registered DesignWare HDMI I2C bus driver
01-01 00:00:01.988 1 1 E imx-lcdifv3 32e80000.lcd-controller: lcdif: failed to get response of echo. Use normal mode.
01-01 00:00:02.007 1 1 I imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops [imx_lcdifv3_crtc])
01-01 00:00:02.018 1 1 I imx-drm display-subsystem: bound imx-lcdifv3-crtc.1 (ops lcdifv3_crtc_ops [imx_lcdifv3_crtc])
01-01 00:00:02.028 1 1 I imx-drm display-subsystem: bound imx-lcdifv3-crtc.2 (ops lcdifv3_crtc_ops [imx_lcdifv3_crtc])
01-01 00:00:02.039 1 1 I imx-drm display-subsystem: bound 32fd8000.hdmi (ops dw_hdmi_imx_ops [dw_hdmi_imx])
01-01 00:00:02.048 1 1 I : [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 0
01-01 00:00:02.079 1 1 I xhci-hcd.0.auto: xHCI Host Controller
01-01 00:00:02.085 1 1 I xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
01-01 00:00:02.094 1 1 I xhci-hcd.0.auto: hcc params 0x0220fe6d hci version 0x110 quirks 0x0000002001010010
01-01 00:00:02.104 1 1 I xhci-hcd.0.auto: irq 247, io mem 0x38200000
01-01 00:00:02.111 1 1 I xhci-hcd.0.auto: xHCI Host Controller
01-01 00:00:02.117 1 1 I xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
01-01 00:00:02.126 1 1 I xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
01-01 00:00:02.133 1 1 I usb1 : New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.15
01-01 00:00:02.142 1 1 I usb1 : New USB device strings: Mfr=3, Product=2, SerialNumber=1
01-01 00:00:02.150 1 1 I usb1 : Product: xHCI Host Controller
01-01 00:00:02.155 1 1 I usb1 : Manufacturer: Linux 5.15.74-gd14ab594eb48-dirty xhci-hcd
01-01 00:00:02.163 1 1 I usb1 : SerialNumber: xhci-hcd.0.auto
01-01 00:00:02.169 1 1 I hub 1-0 : 1.0: USB hub found
01-01 00:00:02.174 1 1 I hub 1-0 : 1.0: 1 port detected
01-01 00:00:02.179 1 1 I usb2 : We don't know the algorithms for LPM for this host, disabling LPM.
01-01 00:00:02.188 1 1 I usb2 : New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.15
01-01 00:00:02.197 1 1 I usb2 : New USB device strings: Mfr=3, Product=2, SerialNumber=1
01-01 00:00:02.205 1 1 I usb2 : Product: xHCI Host Controller
01-01 00:00:02.210 1 1 I usb2 : Manufacturer: Linux 5.15.74-gd14ab594eb48-dirty xhci-hcd
01-01 00:00:02.218 1 1 I usb2 : SerialNumber: xhci-hcd.0.auto
01-01 00:00:02.225 1 1 I hub 2-0 : 1.0: USB hub found
01-01 00:00:02.230 1 1 I hub 2-0 : 1.0: 1 port detected
01-01 00:00:02.240 1 1 W __power_supply_register: Expected proper parent device for 'battery'
01-01 00:00:02.249 1 1 W __power_supply_register: Expected proper parent device for 'usb'
01-01 00:00:02.268 1 1 I : imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 5 mkt segment 0 supported-hw 0x20 0x1
01-01 00:00:02.285 1 1 W ov5640 2-003c: supply DOVDD not found, using dummy regulator
01-01 00:00:02.293 1 1 W ov5640 2-003c: supply AVDD not found, using dummy regulator
01-01 00:00:02.300 1 1 W ov5640 2-003c: supply DVDD not found, using dummy regulator
01-01 00:00:02.355 1 1 E ov5640 2-003c: ov5640_read_reg: error: reg=300a
01-01 00:00:02.361 1 1 E ov5640 2-003c: ov5640_check_chip_id: failed to read chip identifier
01-01 00:00:02.370 1 1 W imx8_isi_hw: module is from the staging directory, the quality is unknown, you have been warned.
01-01 00:00:02.383 1 1 W imx8_isi_mem2mem: module is from the staging directory, the quality is unknown, you have been warned.
01-01 00:00:02.396 1 1 W imx8_isi_capture: module is from the staging directory, the quality is unknown, you have been warned.
01-01 00:00:02.410 1 1 W imx8_capture: module is from the staging directory, the quality is unknown, you have been warned.
01-01 00:00:02.423 1 1 I isi-capture 32e00000.isi: cap_device: deferring 32e00000.isi:cap_device device registration
01-01 00:00:02.433 1 1 I isi-m2m 32e00000.isi: m2m_device: deferring 32e00000.isi:m2m_device device registration
01-01 00:00:02.443 74 74 I usb 1-1 : new high-speed USB device number 2 using xhci-hcd
01-01 00:00:02.450 1 1 I mxc-isi 32e00000.isi: mxc_isi.0 registered successfully
01-01 00:00:02.458 1 1 W imx8_mipi_csi2_sam: module is from the staging directory, the quality is unknown, you have been warned.
01-01 00:00:02.459 8 8 I isi-m2m 32e00000.isi: m2m_device: Register m2m success for ISI.0
01-01 00:00:02.478 1 1 W mxc-mipi-csi2-sam 32e40000.csi: supply mipi-phy not found, using dummy regulator
01-01 00:00:02.488 1 1 E : : mipi_csis_imx8mp_phy_reset, No remote pad found!
01-01 00:00:02.494 1 1 I mxc-mipi-csi2-sam 32e40000.csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 500000000
01-01 00:00:02.510 96 96 I imx-sdma 30bd0000.dma-controller: firmware found.
01-01 00:00:02.516 96 96 I imx-sdma 30bd0000.dma-controller: loaded firmware 4.6
01-01 00:00:02.518 8 8 I 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 36, base_baud = 5000000) is a IMX
01-01 00:00:02.534 8 8 I 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 35, base_baud = 5000000) is a IMX
01-01 00:00:02.535 32 32 I imx-sdma 30e10000.dma-controller: firmware found.
01-01 00:00:02.551 66 66 E : trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1
01-01 00:00:02.551 96 96 E : trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1
01-01 00:00:02.559 32 32 E : trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1
01-01 00:00:02.559 43 43 E : trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1
01-01 00:00:02.567 1 1 I : trusty trusty: trusty-log not supported on secure side.
01-01 00:00:02.593 1 1 E trusty-virtio trusty: trusty-virtio: trusty_load_device_descr: virtio get descr returned (-1)
01-01 00:00:02.603 1 1 E trusty-virtio trusty: trusty-virtio: failed (-19) to load device descr
01-01 00:00:02.611 1 1 E trusty-virtio trusty: trusty-virtio: Failed to add virtio devices
01-01 00:00:02.619 1 1 W basler_camera_driver_vvcam: loading out-of-tree module taints kernel.
01-01 00:00:02.631 74 74 I usb 1-1 : New USB device found, idVendor=1d5c, idProduct=5510, bcdDevice= 1.02
01-01 00:00:02.631 1 1 W imx8_media_dev: module is from the staging directory, the quality is unknown, you have been warned.
01-01 00:00:02.640 74 74 I usb 1-1 : New USB device strings: Mfr=1, Product=2, SerialNumber=0
01-01 00:00:02.658 74 74 I usb 1-1 : Product: Frescologic USB2.0 HUB
01-01 00:00:02.659 1 1 I mx8-img-md: Registered mxc_isi.0.capture as /dev/video1
01-01 00:00:02.664 74 74 I usb 1-1 : Manufacturer: Frescologic
01-01 00:00:02.671 1 1 I : unregister ISI channel: mxc_isi.0
01-01 00:00:02.683 1 1 I : enter viv_dwe_init_module
01-01 00:00:02.690 1 1 I : enter viv_isp_init_module
01-01 00:00:02.697 1 1 I : enter viv_video_init_module
01-01 00:00:02.710 74 74 I hub 1-1 : 1.0: USB hub found
01-01 00:00:02.715 74 74 I hub 1-1 : 1.0: 5 ports detected
01-01 00:00:02.731 1 1 I cfg80211: Loading compiled-in X.509 certificates for regulatory database
01-01 00:00:02.742 1 1 I cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
01-01 00:00:02.773 88 88 I usb 2-1 : new SuperSpeed USB device number 2 using xhci-hcd
01-01 00:00:02.808 88 88 I usb 2-1 : New USB device found, idVendor=1d5c, idProduct=5500, bcdDevice= 1.02
01-01 00:00:02.812 100 100 I random : fsck.f2fs: uninitialized urandom read (40 bytes read)
01-01 00:00:02.817 88 88 I usb 2-1 : New USB device strings: Mfr=1, Product=2, SerialNumber=0
01-01 00:00:02.817 88 88 I usb 2-1 : Product: Frescologic USB3.1Gen2 HUB
01-01 00:00:02.817 88 88 I usb 2-1 : Manufacturer: Frescologic
01-01 00:00:02.845 88 88 I hub 2-1 : 1.0: USB hub found
01-01 00:00:02.846 1 1 I fsck.f2fs: linker: Warning: failed to find generated linker configuration from "/linkerconfig/ld.config.txt"
01-01 00:00:02.850 88 88 I hub 2-1 : 1.0: 4 ports detected
01-01 00:00:02.851 100 100 I random : fsck.f2fs: uninitialized urandom read (40 bytes read)
01-01 00:00:02.851 100 100 I random : fsck.f2fs: uninitialized urandom read (4 bytes read)
01-01 00:00:02.861 1 1 I fsck.f2fs: WARNING: linker: Warning: failed to find generated linker configuration from "/linkerconfig/ld.config.txt"
01-01 00:00:02.892 100 100 I : fsck.f2fs (100) used greatest stack depth: 12528 bytes left
01-01 00:00:02.893 1 1 I fsck.f2fs: Info: Fix the reported corruption.
01-01 00:00:02.907 1 1 I fsck.f2fs: Info: not exist /proc/version!
01-01 00:00:02.912 1 1 I fsck.f2fs: Info: Segments per section = 1
01-01 00:00:02.918 1 1 I fsck.f2fs: Info: Sections per zone = 1
01-01 00:00:02.924 1 1 I fsck.f2fs: Info: sector size = 512
01-01 00:00:02.929 1 1 I fsck.f2fs: Info: total sectors = 131072 (64 MB)
01-01 00:00:02.935 1 1 I fsck.f2fs: Info: MKFS version
01-01 00:00:02.940 1 1 I fsck.f2fs: "5.15.74-gd14ab594eb48-dirty"
01-01 00:00:02.996 1 1 I F2FS-fs (mmcblk2p10): Mounted with checkpoint version = 3e52e044
01-01 00:00:03.058 1 1 I device-mapper: verity: sha256 using implementation "sha256-ce"
01-01 00:00:03.071 1 1 I erofs : (device dm-5): mounted with root inode @ nid 59.
01-01 00:00:03.084 1 1 I device-mapper: verity: sha256 using implementation "sha256-ce"
01-01 00:00:03.097 1 1 I erofs : (device dm-6): mounted with root inode @ nid 38.
01-01 00:00:03.108 1 1 I device-mapper: verity: sha256 using implementation "sha256-ce"
01-01 00:00:03.120 1 1 I erofs : (device dm-7): mounted with root inode @ nid 42.
01-01 00:00:03.130 1 1 I device-mapper: verity: sha256 using implementation "sha256-ce"
01-01 00:00:03.143 1 1 I erofs : (device dm-8): mounted with root inode @ nid 39.
01-01 00:00:03.152 1 1 I device-mapper: verity: sha256 using implementation "sha256-ce"
01-01 00:00:03.165 1 1 I erofs : (device dm-9): mounted with root inode @ nid 39.
01-01 00:00:03.218 1 1 W printk : init: 14 output lines suppressed due to ratelimiting
01-01 00:00:03.225 1 1 W printk : init: 203 output lines suppressed due to ratelimiting
01-01 00:00:03.340 74 74 I usb 1-1.4: new full-speed USB device number 3 using xhci-hcd
01-01 00:00:03.388 1 1 I init : Opening SELinux policy
01-01 00:00:03.396 1 1 I init : Falling back to standard signature check. TODO implementent support for fsverity SEPolicy.
01-01 00:00:03.407 1 1 I init : Error: Apex SEPolicy failed signature check
01-01 00:00:03.414 1 1 I init : Loading APEX Sepolicy from /system/etc/selinux/apex/SEPolicy.zip
01-01 00:00:03.422 1 1 E init : Failed to open package /system/etc/selinux/apex/SEPolicy.zip: No such file or directory
01-01 00:00:03.444 1 1 I init : Loading SELinux policy
01-01 00:00:03.450 74 74 I usb 1-1.4: New USB device found, idVendor=0712, idProduct=0009, bcdDevice= 2.00
01-01 00:00:03.459 74 74 I usb 1-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=3
01-01 00:00:03.467 74 74 I usb 1-1.4: Product: WaveShare
01-01 00:00:03.472 74 74 I usb 1-1.4: Manufacturer: WaveShare
01-01 00:00:03.473 1 1 I SELinux : Permission bpf in class capability2 not defined in policy.
01-01 00:00:03.477 74 74 I usb 1-1.4: SerialNumber: 000000000089
01-01 00:00:03.485 1 1 I SELinux : Permission checkpoint_restore in class capability2 not defined in policy.
01-01 00:00:03.500 1 1 I SELinux : Permission bpf in class cap2_userns not defined in policy.
01-01 00:00:03.508 1 1 I SELinux : Permission checkpoint_restore in class cap2_userns not defined in policy.
01-01 00:00:03.518 1 1 I SELinux : Class mctp_socket not defined in policy.
01-01 00:00:03.524 1 1 I SELinux : the above unknown classes and permissions will be denied
01-01 00:00:03.539 1 1 I SELinux : policy capability network_peer_controls=1
01-01 00:00:03.546 1 1 I SELinux : policy capability open_perms=1
01-01 00:00:03.551 74 74 I input : WaveShare WaveShare as /devices/platform/soc@0/32f10108.usb/38200000.usb/xhci-hcd.0.auto/usb1/1-1/1-1.4/1-1.4:1.0/0003:0712:0009.0001/input/input1
01-01 00:00:03.552 1 1 I SELinux : policy capability extended_socket_class=1
01-01 00:00:03.567 74 74 I hid-multitouch 0003: 0712:0009.0001: input,hidraw0: USB HID v1.11 Device [WaveShare WaveShare] on usb-xhci-hcd.0.auto-1.4/input0
01-01 00:00:03.574 1 1 I SELinux : policy capability always_check_network=0
01-01 00:00:03.574 1 1 I SELinux : policy capability cgroup_seclabel=0
01-01 00:00:03.574 1 1 I SELinux : policy capability nnp_nosuid_transition=1
01-01 00:00:03.606 1 1 I SELinux : policy capability genfs_seclabel_symlinks=0
01-01 00:00:03.613 1 1 I SELinux : policy capability ioctl_skip_cloexec=0
01-01 00:00:03.878 1 1 I selinux : SELinux: Loaded file_contexts
01-01 00:00:03.883 1 1 I selinux :
01-01 00:00:03.904 1 1 I random : init: uninitialized urandom read (40 bytes read)
01-01 00:00:03.927 1 1 I random : init: uninitialized urandom read (40 bytes read)
01-01 00:00:03.934 1 1 I random : init: uninitialized urandom read (4 bytes read)
01-01 00:00:03.944 1 1 I init : init second stage started!
01-01 00:00:04.002 1 1 I init : Using Android DT directory /proc/device-tree/firmware/android/
01-01 00:00:04.016 1 1 W init : Couldn't load property file '/system_dlkm/etc/build.prop': open() failed: No such file or directory: No such file or directory
01-01 00:00:04.029 1 1 W init : Couldn't load property file '/vendor/default.prop': open() failed: No such file or directory: No such file or directory
01-01 00:00:04.047 1 1 W init : Couldn't load property file '/odm_dlkm/etc/build.prop': open() failed: No such file or directory: No such file or directory
01-01 00:00:04.063 1 1 I init : Setting product property ro.product.brand to 'Android' (from ro.product.product.brand)
01-01 00:00:04.074 1 1 I init : Setting product property ro.product.device to 'lec_imx8mp' (from ro.product.product.device)
01-01 00:00:04.084 1 1 I init : Setting product property ro.product.manufacturer to 'nxp' (from ro.product.product.manufacturer)
01-01 00:00:04.095 1 1 I init : Setting product property ro.product.model to 'lec_imx8mp' (from ro.product.product.model)
01-01 00:00:04.106 1 1 I init : Setting product property ro.product.name to 'lec_imx8mp' (from ro.product.product.name)
01-01 00:00:04.349 126 126 E linkerconfig: Unable to access VNDK APEX at path: /apex/com.android.vndk.v33: No such file or directory
01-01 00:00:04.361 126 126 E linkerconfig: Unable to access VNDK APEX at path: /apex/com.android.vndk.v33: No such file or directory
01-01 00:00:04.376 126 126 I : linkerconfig (126) used greatest stack depth: 11120 bytes left
01-01 00:00:04.416 127 127 I ueventd : ueventd started!
01-01 00:00:04.425 127 127 I selinux : SELinux: Loaded file_contexts
01-01 00:00:04.430 127 127 I selinux :
01-01 00:00:04.435 127 127 I ueventd : Parsing file /system/etc/ueventd.rc...
01-01 00:00:04.442 127 127 I ueventd : Added '/vendor/etc/ueventd.rc' to import list
01-01 00:00:04.449 127 127 I ueventd : Added '/odm/etc/ueventd.rc' to import list
01-01 00:00:04.457 127 127 I ueventd : Parsing file /vendor/etc/ueventd.rc...
01-01 00:00:04.464 127 127 I ueventd : Parsing file /odm/etc/ueventd.rc...
01-01 00:00:04.470 127 127 I ueventd : Unable to read config file '/odm/etc/ueventd.rc': open() failed: No such file or directory
01-01 00:00:04.493 128 128 I apexd : Bootstrap subcommand detected
01-01 00:00:04.499 128 128 E cutils-trace: Error opening trace file: No such file or directory (2)
01-01 00:00:04.688 128 128 I apexd : wait for '/dev/loop-control' took 145ms
01-01 00:00:04.724 128 128 I apexd : Pre-allocated 16 loopback devices
01-01 00:00:04.730 128 128 I apexd : Scanning /system/apex for pre-installed ApexFiles
01-01 00:00:04.738 128 128 I apexd : Found pre-installed APEX /system/apex/com.android.adbd.capex
01-01 00:00:04.753 128 128 I apexd : Found pre-installed APEX /system/apex/com.android.adservices.capex
01-01 00:00:04.764 128 128 I apexd : Found pre-installed APEX /system/apex/com.android.apex.cts.shim.apex
01-01 00:00:04.773 128 128 I apexd : Found pre-installed APEX /system/apex/com.android.appsearch.apex
01-01 00:00:04.782 128 128 I apexd : Found pre-installed APEX /system/apex/com.android.art.capex
01-01 00:00:04.847 162 162 I loop0 : detected capacity change from 0 to 96704
01-01 00:00:04.855 161 161 I loop1 : detected capacity change from 0 to 16240
01-01 00:00:04.886 127 127 I ueventd : Coldboot took 0.403 seconds
01-01 00:00:04.936 161 161 I EXT4-fs (loop1): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:04.946 162 162 I EXT4-fs (loop0): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:04.955 161 161 I loop2 : detected capacity change from 0 to 74600
01-01 00:00:04.963 162 162 I loop3 : detected capacity change from 0 to 1728
01-01 00:00:05.024 161 161 I EXT4-fs (loop2): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:05.031 162 162 I EXT4-fs (loop3): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:05.057 128 128 W printk : apexd: 41 output lines suppressed due to ratelimiting
01-01 00:00:05.065 128 128 I : apexd (128) used greatest stack depth: 10736 bytes left
01-01 00:00:05.092 169 169 I random : linkerconfig: uninitialized urandom read (40 bytes read)
01-01 00:00:05.101 169 169 I random : linkerconfig: uninitialized urandom read (4 bytes read)
01-01 00:00:05.108 169 169 I random : linkerconfig: uninitialized urandom read (4 bytes read)
01-01 00:00:05.220 170 170 W : getrandom indicates that the entropy pool has not been initialized. Rather than continue with poor entropy, this process will block until entropy is available.
01-01 00:00:06.932 0 0 I [ C0] random: crng init done
01-01 00:00:06.936 0 0 I [ C0] random: 63 urandom warning(s) missed due to ratelimiting
01-01 00:00:07.173 174 174 W prng_seeder: Hanging forever because setup failed: hwrng.read_exact in new
01-01 00:00:07.184 174 174 W Caused by:
01-01 00:00:07.187 174 174 W : No such device (os error 19)
01-01 00:00:07.276 178 178 F wlan : Loading MWLAN driver
01-01 00:00:07.281 178 178 F wlan : Register to Bus Driver...
01-01 00:00:07.286 178 178 F wlan : Register to SDIO_MMC Bus Driver
01-01 00:00:07.292 178 178 F : vendor=0x02DF device=0x9141 class=0 function=1
01-01 00:00:07.298 178 178 F : Attach moal handle ops, card interface type: 0x104
01-01 00:00:07.305 178 178 F : rps set to 0 from module param
01-01 00:00:07.311 178 178 F SD8997 : init module param from usr cfg
01-01 00:00:07.317 178 178 F card_type: SD8997, config block: 0
01-01 00:00:07.322 178 178 F : cfg80211_wext=0xf
01-01 00:00:07.326 178 178 F : sta_name=wlan
01-01 00:00:07.329 178 178 F : uap_name=wlan
01-01 00:00:07.332 178 178 F : wfd_name=p2p
01-01 00:00:07.336 178 178 F : max_vir_bss=1
01-01 00:00:07.339 178 178 F : cal_data_cfg=none
01-01 00:00:07.342 178 178 F : ps_mode = 1
01-01 00:00:07.346 178 178 F : auto_ds = 1
01-01 00:00:07.349 178 178 F : host_mlme=enable
01-01 00:00:07.352 178 178 F : fw_name=nxp/sdsd8997_combo_v4.bin
01-01 00:00:07.358 178 178 F SDIO : max_segs=128 max_seg_size=65535
01-01 00:00:07.363 178 178 F : rx_work=1 cpu_num=4
01-01 00:00:07.367 178 178 W : Attach mlan adapter operations.card_type is 0x104.
01-01 00:00:07.379 178 178 W wlan : Enable TX SG mode
01-01 00:00:07.383 178 178 W wlan : Enable RX SG mode
01-01 00:00:07.394 178 178 F Request firmware: nxp/sdsd8997_combo_v4.bin
01-01 00:00:07.415 178 178 W : mlan_dnld_fw
01-01 00:00:07.423 178 178 W : Check if firmware is already running
01-01 00:00:07.429 178 178 W wlan_sdio_check_fw_status: Wait for firmware initialization event
01-01 00:00:07.486 1 1 E pstore : crypto_comp_decompress failed, ret = -22!
01-01 00:00:07.503 1 1 I : Registered swp emulation handler
01-01 00:00:07.610 186 186 I logd.auditd: start
01-01 00:00:07.613 193 193 I watchdogd: watchdogd started (interval 10, margin 20)!
01-01 00:00:07.644 186 186 I logd : Loaded bug_map file: /vendor/etc/selinux/selinux_denial_metadata
01-01 00:00:07.653 186 186 I logd : Loaded bug_map file: /system/etc/selinux/bug_map
01-01 00:00:07.809 1 1 I zram0 : detected capacity change from 0 to 1228800
01-01 00:00:07.842 1 1 I mkswap : Swapspace size: 614396k, UUID=610c7397-03f1-42a0-926f-30c0925d3fad
01-01 00:00:07.872 1 1 I : Adding 614396k swap on /dev/block/zram0. Priority:-2 extents:1 across:614396k SS
01-01 00:00:08.033 224 224 D vdc : Waited 0ms for vold
01-01 00:00:08.086 233 233 D vdc : Waited 0ms for vold
01-01 00:00:08.217 201 201 I fsck.f2fs: Info: Fix the reported corruption.
01-01 00:00:08.223 201 201 I fsck.f2fs: Info: not exist /proc/version!
01-01 00:00:08.229 201 201 I fsck.f2fs: Info: Segments per section = 1
01-01 00:00:08.235 201 201 I fsck.f2fs: Info: Sections per zone = 1
01-01 00:00:08.240 201 201 I fsck.f2fs: Info: sector size = 4096
01-01 00:00:08.246 201 201 I fsck.f2fs: Info: total sectors = 6197760 (24210 MB)
01-01 00:00:08.252 201 201 I fsck.f2fs: Info: MKFS version
01-01 00:00:08.257 201 201 I fsck.f2fs: "5.15.74-gd14ab594eb48-dirty"
01-01 00:00:08.263 201 201 I fsck.f2fs: Info: FSCK version
01-01 00:00:08.268 201 201 I fsck.f2fs: from "5.15.74-gd14ab594eb48-dirty"
01-01 00:00:08.358 201 201 I F2FS-fs (dm-38): Using encoding defined by superblock: utf8-12.1.0 with flags 0x0
01-01 00:00:08.453 201 201 I F2FS-fs (dm-38): recover_inode: ino = 317d, name = , inline = 21
01-01 00:00:08.462 201 201 I F2FS-fs (dm-38): recover_data: ino = 317d (i_size: recover) recovered = 1, err = 0
01-01 00:00:08.472 201 201 I F2FS-fs (dm-38): recover_inode: ino = 1d1a, name = , inline = 21
01-01 00:00:08.480 201 201 I F2FS-fs (dm-38): recover_data: ino = 1d1a (i_size: recover) recovered = 0, err = 0
01-01 00:00:08.490 201 201 I F2FS-fs (dm-38): recover_inode: ino = 317e, name = , inline = 21
01-01 00:00:08.499 201 201 I F2FS-fs (dm-38): recover_dentry: ino = 317e, name = , dir = 177a, err = 0
01-01 00:00:08.509 201 201 I F2FS-fs (dm-38): recover_data: ino = 317e (i_size: recover) recovered = 1, err = 0
01-01 00:00:08.518 201 201 I F2FS-fs (dm-38): recover_inode: ino = 3177, name = , inline = 21
01-01 00:00:08.527 201 201 I F2FS-fs (dm-38): recover_data: ino = 3177 (i_size: recover) recovered = 1, err = 0
01-01 00:00:08.536 201 201 I F2FS-fs (dm-38): recover_inode: ino = 1d1a, name = , inline = 21
01-01 00:00:08.545 201 201 I F2FS-fs (dm-38): recover_data: ino = 1d1a (i_size: recover) recovered = 1, err = 0
01-01 00:00:08.561 201 201 I F2FS-fs (dm-38): checkpoint: version = 276aec00
01-01 00:00:08.568 201 201 I F2FS-fs (dm-38): Mounted with checkpoint version = 276aec00
01-01 00:00:08.569 178 178 W Wlan : FW download over, firmwarelen=623240 downloaded 623240
01-01 00:00:08.582 178 178 W wlan_sdio_check_fw_status: Wait for firmware initialization event
01-01 00:00:08.647 259 259 D vdc : Waited 0ms for vold
01-01 00:00:08.673 1 1 I fscrypt : AES-256-CTS-CBC using implementation "cts-cbc-aes-ce"
01-01 00:00:08.776 201 201 E vold : keystore2 Keystore earlyBootEnded returned service specific error: -68
01-01 00:00:08.836 199 199 I logd : logd reinit
01-01 00:00:08.843 199 199 E logd : FrameworkListener: read() failed (Connection reset by peer)
01-01 00:00:08.843 268 268 I apexd : Scanning /system/apex for pre-installed ApexFiles
01-01 00:00:08.859 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.adbd.capex
01-01 00:00:08.867 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.adservices.capex
01-01 00:00:08.877 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.apex.cts.shim.apex
01-01 00:00:08.886 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.appsearch.apex
01-01 00:00:08.895 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.art.capex
01-01 00:00:08.904 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.btservices.apex
01-01 00:00:08.913 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.car.framework.apex
01-01 00:00:08.922 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.cellbroadcast.capex
01-01 00:00:08.931 268 268 I apexd : Found pre-installed APEX /system/apex/com.android.conscrypt.capex
01-01 00:00:09.069 270 270 I loop4 : detected capacity change from 0 to 41784
01-01 00:00:09.077 271 271 I loop5 : detected capacity change from 0 to 6952
01-01 00:00:09.139 270 270 I EXT4-fs (loop4): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.140 271 271 I EXT4-fs (loop5): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.152 270 270 I loop6 : detected capacity change from 0 to 12952
01-01 00:00:09.165 271 271 I loop7 : detected capacity change from 0 to 536
01-01 00:00:09.219 270 270 I EXT4-fs (loop6): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.234 270 270 I loop8 : detected capacity change from 0 to 1728
01-01 00:00:09.237 271 271 I EXT4-fs (loop7): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.254 271 271 I loop9 : detected capacity change from 0 to 536
01-01 00:00:09.296 270 270 I EXT4-fs (loop8): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.307 270 270 I loop10 : detected capacity change from 0 to 74600
01-01 00:00:09.341 271 271 I EXT4-fs (loop9): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.352 271 271 I loop11 : detected capacity change from 0 to 96704
01-01 00:00:09.371 270 270 I EXT4-fs (loop10): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.383 270 270 I loop12 : detected capacity change from 0 to 3920
01-01 00:00:09.411 271 271 I EXT4-fs (loop11): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.420 178 178 F : WLAN FW is active
01-01 00:00:09.422 271 271 I loop13 : detected capacity change from 0 to 16240
01-01 00:00:09.425 178 178 F : on_time is 9252720625
01-01 00:00:09.442 270 270 I EXT4-fs (loop12): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.454 270 270 I loop14 : detected capacity change from 0 to 536
01-01 00:00:09.476 66 66 W : fw_cap_info=0x18fcffa3, dev_cap_mask=0xffffffff
01-01 00:00:09.483 66 66 W : max_p2p_conn = 8, max_sta_conn = 8
01-01 00:00:09.500 178 178 F : Register NXP 802.11 Adapter wlan0
01-01 00:00:09.506 178 178 F wlan : wlan%d set max_mtu 2000
01-01 00:00:09.511 271 271 I EXT4-fs (loop13): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.512 178 178 F : Register NXP 802.11 Adapter wlan1
01-01 00:00:09.522 271 271 I loop15 : detected capacity change from 0 to 1536
01-01 00:00:09.523 270 270 I EXT4-fs (loop14): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.531 178 178 F : Register NXP 802.11 Adapter p2p0
01-01 00:00:09.533 270 270 I loop16 : detected capacity change from 0 to 17256
01-01 00:00:09.542 178 178 F wlan : version = SD8997----16.68.1.p197-MM5X16368.p2-GPL-(FP92)
01-01 00:00:09.562 178 178 E WLAN : SDIO Driver Registration SUCCESS
01-01 00:00:09.568 178 178 F wlan : Register to Bus Driver Done
01-01 00:00:09.573 178 178 F wlan : Driver loaded successfully
01-01 00:00:09.584 178 178 F BT : Loading driver
01-01 00:00:09.597 178 178 F : BT FW is active(0)
01-01 00:00:09.601 270 270 I device-mapper: verity: sha256 using implementation "sha256-ce"
01-01 00:00:09.601 178 178 F BT : FW already downloaded!
01-01 00:00:09.619 271 271 I EXT4-fs (loop15): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.630 271 271 I loop17 : detected capacity change from 0 to 40512
01-01 00:00:09.630 178 178 F BT : Create /dev/mbtchar0
01-01 00:00:09.640 270 270 I EXT4-fs (dm-36): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.653 270 270 I loop18 : detected capacity change from 0 to 17128
01-01 00:00:09.677 271 271 I device-mapper: verity: sha256 using implementation "sha256-ce"
01-01 00:00:09.705 178 178 F BT : Create /dev/mdebugchar0
01-01 00:00:09.709 270 270 I device-mapper: verity: sha256 using implementation "sha256-ce"
01-01 00:00:09.728 271 271 I EXT4-fs (dm-35): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.732 270 270 I EXT4-fs (dm-34): mounted filesystem without journal. Opts: (null). Quota mode: none.
01-01 00:00:09.734 270 270 I loop19 : detected capacity change from 0 to 29504
01-01 00:00:09.744 178 178 F BT : Driver loaded successfully

Re: 88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"

hi, 

Thank you so much for the reply. 

I am working on Android 13 with kernel version 5.15.74 . i have ported the mbt8xxx driver from android 11 to android 13. It is working fine in my device, but after bluetooth connection the bluetooth is crashing after going through the dmesg i am getting the error as I mentioned above

Re: 88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"

Hello @jeevanefx123 

AW-CM276 have no SD-BT support. Your may use sd-uart firmware.

shaun_wu_0-1728369857718.png


Best Regards

Shaun

Re: 88w8997 Wifi driver IOCTL issue with firmware version "sdsd8997_combo_v4.bin"
Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:24 PM
Updated by: