1967483_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1967483_en-US

1967483_en-US

Is there any difference between the USB1 and USB2 ports on the i.MX 8M PLUS?

Hi all,

Q1) According to the documentation provided by NXP, the two USB ports on the i.MX8MPLUS appear to have the same functionality. Is our understanding correct?

Q2) Does the USB Serial download mode work on either port?
       *Is there a setting to prioritize one port over the other?

Thanks,
George

i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlusi.MX 8M | i.MX 8M Mini | i.MX 8M NanoRe: Is there any difference between the USB1 and USB2 ports on the i.MX 8M PLUS?

Hello @Bio_TICFSL,

Thank you for your answer.

I have confirmed that Serial-Download mode does indeed work on both USB ports using the IMX8MP-EVK.
It seems that which port is used for Serial Download is determined by USBx_VBUS.

Thanks,
George

Re: Is there any difference between the USB1 and USB2 ports on the i.MX 8M PLUS?

Hello,

a) Yes both works as the same functionality

b) Yes, Please refer to the https://www.nxp.com/webapp/Download?colCode=IMX8MMEVKHUG  for details like switch settings and steps to follow for serial download mode.


Regards

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:25 PM
Updated by: