1966552_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1966552_en-US

1966552_en-US

[Android Automotive 12] Release 12.1.0_1.1.0 on i.MX 8QuadMax Audio fails

Hello community,

All of three releases of Android Automotive 12 for i.MX 8 cannot play any sound.
The same board is confirmed working when running an Android Automotive 13 image.

The audio jack is connected to a pair of speakers, and the kitchen sink app is used to play sound. I also tried with an YouTube video.

Here are related errors from logcat

11:30:08.894   385-4621  audio_hw_primary    android.hardware.audio.service  I  start_output_stream: primary: 1, out: 0xe6042d70, device: 16777216, address: bus0_media_out, mode: 0, flags 0x2
11:30:08.894   385-4621  audio_hw_primary    android.hardware.audio.service  I  select_output_device(), headphone 0 ,headset 0 ,speaker 2
11:30:08.894   385-4621  audio_hw_primary    android.hardware.audio.service  E  Failed to find card from bus 'bus0_media_out'
11:30:08.894   385-4621  audio_hw_primary    android.hardware.audio.service  D  start_output_stream: pcm_open: card: -1, pcm_device_id: 0, rate: 48000, channel: 2, format: 0, period_size: 0xc0, flag: 9
11:30:08.894   385-4621  audio_hw_primary    android.hardware.audio.service  E  start_output_stream: Invalid PCM card id: -1

 Full log export from Android Studio's logcat is attached. The .logcat file can be used to import to Android Studio for better viewing.

Re: [Android Automotive 12] Release 12.1.0_1.1.0 on i.MX 8QuadMax Audio fails

I am able to confirm audio from the audio jack via kitchen sink app -> volume test. In the app, I only hear audio when testing bus #1.


It looks like I am supposed to modify tags in device code if I want to route all audio to the audio jack.

Re: [Android Automotive 12] Release 12.1.0_1.1.0 on i.MX 8QuadMax Audio fails

I have read more about audio on this thread.

It looks like it is the way to go if I want to route all audio to the audio jack.

This is weird and luckily this behavior does not exist in newer Android releases.

Tags (1)
No ratings
Version history
Last update:
‎11-22-2025 05:50 AM
Updated by: