1962539_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1962539_en-US

1962539_en-US

LPCMP external SAMPLE input

Hi,

When I set CCR1[SAMPLE_EN] to be 1, which clock source would be used?
Is the external signal source an actual pin input or is it set somewhere else?”

S32K3X4EVB-T172 , #LPCMP, #RTD

Jack_Hsu_0-1727340085947.png

Jack_Hsu_1-1727340681853.png


Re: LPCMP external SAMPLE input

Hi @Jack_Hsu 

When CCR1[SAMPLE_EN]=1, the WINDOW/SAMPLE signal acts as the Sampling Clock of the Filter Block. The external SAMPLE input signal is an output pulse generated via TRGMUX. See the LPCMP_Sample/Window input in the TRGMUX connectivity file attached to the S32K3xx Reference Manual, Rev. 8. 


BR, VaneB

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 08:34 PM
更新者: