1961563_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1961563_en-US

1961563_en-US

RT1170EVKB USB-RNDIS automatic recognition


Hi, I successfully communicated with a Windows PC using the VNIC sample and lwIP sample on the RT1170EVKB.

However, to enable communication on the Windows PC, I had to install the "fsl_rndis.inf" file for the Ethernet device to be created.

The issue is that this works on Windows, but I'm not sure how to use the RNDIS functionality on Linux (such as Ubuntu).

I hope RNDIS will be automatically recognized by all operating systems.

Is there a way to enable RNDIS mode on operating systems other than Windows, such as Linux?

Best regards,

Re: RT1170EVKB USB-RNDIS automatic recognition

I have confirmed that the Ethernet device is automatically recognized on UBUNTU.

I would like to cancel this question.

Best regards,

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 08:36 PM
更新者: