I am currently working on a project that involves integrating WiFi module using the IW612 module with an STM32 micro-controller and I would appreciate your guidance on the integration process .
Could you please provide any documentation or resources that detail the following :
1. Recommended software libraries or SDKs for the STM32.
2. Example code for establishing a WiFi connection.
3. Any specific configuration settings.
Hi, @komal21
Thanks for your feedback.
Then would you mind me closing this case by mark my answer as accepted solution?
Best regards,
Christine.
Thank you for your valuable guidance.
Hi, @komal21
Thanks for your reply.
I am very sorry for the inconvenience, we do not have the special driver for STM32 MCU.
The only way is porting by yourself by referring our I.MX RT platforms running RTOS:
Getting Started with NXP-based Wireless Modules on i.MX RT Platforms Running RTOS - User manual
Or you can think about our RW612 which has integrated MCU and also it can support Wi-Fi6, BLE and Thread.
Best regards,
Christine.
can we interface this IW612 with STM32 it is possible?
NXP provide any driver so using of that we can Interface STM32 MCU with IW612?
Hi, @komal21
Anything else I can for you on this case?
Best regards,
Christine.
Hi, @komal21
Anything else I can for you on this case?
Best regards,
Christine.
Hi, @komal21
Thanks for creating case to us.
We do not have special guidance for STM32 because it is not our NXP own MCU.
But for your reference, this user manual should be helpful for you:
And to configure Wi-Fi/Bluetooth features like establishing connections and configurations based on MCU platform, you can refer to this user manual:
Best regards,
Christine.