1952872_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1952872_en-US

1952872_en-US

s32k312 pwm period & icu configuration

Hello, I am currently working with the PWM input and capture functions of the s32k312, and I have a few questions I would like to confirm with you:

Regarding the calculation of PWM output frequency: Is the formula used as follows to determine the frequency?
Frequency = core_clk / (master bus prescaler) / (clock prescaler) / tick
For example: Frequency = 120MHZ / 1 / 12 / 5000 = 200HZ

微信图片_20240912102157.png微信图片_20240912102203.png
When capturing PWM period and duty cycle through the ICU, does the ICU start capturing immediately after initialization, and is there a running cycle for this process?

Re: s32k312 pwm period & icu configuration

Emios_Pwm_Ip_SetDutyCycle is different from Pwm_SetDutyCycle.
Your understanding is suitable for Pwm_SetDutyCycle:
0x0000 means 0%
0x8000 means 100%

But the duty cycle of Emios_Pwm_Ip_SetDutyCycle is calculated as follows: NewDutyCycle/Period[ticks]
3276/50000=6.55%
6553/20000=32.765%
It matches your test results.

Re: s32k312 pwm period & icu configuration

Alright, I understand. I'm currently testing, thank you. Additionally, I have one more question regarding the duty cycle. I'm not sure if my calculations are correct, so I would appreciate your guidance. I'm currently using the function Emios_Pwm_Ip_SetDutyCycle(uint8 Instance, uint8 Channel, Emios_Pwm_Ip_DutyType NewDutyCycle) to set the duty cycle:

When I set the frequency to 200Hz and pass NewDutyCycle=3276.8, the duty cycle measured by the oscilloscope is not 10% but 6.5%.
When I set the frequency to 500Hz and pass NewDutyCycle=6553.6, the duty cycle is not 20% but 32%.
Can you please tell me where my configuration might be incorrect?"

微信图片_20240914135048.png微信图片_20240914135242.jpg微信图片_20240914135252.jpg

Re: s32k312 pwm period & icu configuration

Hi

Seems that emios is configured as OPWFMB mode.  Clock Divider Value in Emios_Mcl_Ip is used to calculate PWM frequency.

Frequency = core_clk / (Clock Divider Value) / (clock prescaler) / tick

Please verify it by testing.

Emios Mcl Clock Divider Value.png

/*Start measuring */
Emios_Icu_Ip_StartSignalMeasurement(EMIOS1, EMIOS_ch1);
 
Emios_Icu_Ip_GetInputState(EMIOS1, EMIOS_ch1);
/* Get captured duty-cycle and period*/
Emios_Icu_Ip_GetDutyCycleValues(EMIOS1, EMIOS_ch1, &ic_result_temp);
 
/* If captured */
if(ic_result_temp.PeriodTime)
{
/* Stop measuring */
Emios_Icu_Ip_StopSignalMeasurement(EMIOS1, EMIOS_ch1);
captured = 1;
}

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 08:47 PM
更新人: