Hi,
Does anyone have information on the size (surface and thickness) of the active part of the silicon plate which acts as a membrane for pressure measurement?
Thanks
Hi Jean-Luc,
we have an application note dealing with output noise and recommended techniques to mitigate the output oscillations. Please find it attached.
With Best Regards,
Jozef
Thanks Josef.
I test the response of this sensor to a pressure step and I observe damped oscillations of the output voltage. The frequency is about 100 Hz. This frequency seems a little low when I compare it to the natural frequency of a silicon membrane of 1mm^2 x 0.001mm which is of the order of 2500 Hz. Have you ever known of such oscillations?
Sincerely,
Hi Jean-Luc,
I have checked available documents and older cases. Unfortunately I couldn't the requested MPX5010DP inner silicone plate size. We do not have this value.
I apologize for inconvenience.
With Best Regards,
Jozef