1951073_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1951073_en-US

1951073_en-US

Which BSP to use to run Xen on i.MX 8M Plus? L4.14 is discontinued, and newer versions don't seem to

Hello,

I'm trying to set up Xen hypervisor on the i.MX 8M Plus platform. I noticed that the L4.14 BSP has been discontinued, and after reviewing the newer BSP versions (e.g., L5.4.x or L5.10.x), it appears they don't officially support Xen.

Could anyone clarify which BSP version I should use to successfully run Xen on the i.MX 8M Plus? Are there any recommended workarounds or specific patches that I can apply to the newer BSPs to enable Xen?

Thanks in advance for your help!

i.MX 8M | i.MX 8M Mini | i.MX 8M NanoLinuxRe: Which BSP to use to run Xen on i.MX 8M Plus? L4.14 is discontinued, and newer versions don't see

Hello @mkchaaru 

I hope you are doing well.


Unfortunately, as you said, i.MX8MP does not support XEN, also, there is not an official patched or ways tu run it on a new BSP.

There is an alternative to XEN, you can take a look to Jailhouse that is supported on latest BSPs.


Apologies for any inconvenience.


Best regards,

Salas. 

Re: Which BSP to use to run Xen on i.MX 8M Plus? L4.14 is discontinued, and newer versions don't see

hi @Manuel_Salas  i am using MCIMX8QM soc 

does this support XEN hypervisor ?

标记 (1)
无评分
版本历史
最后更新:
‎03-18-2026 03:41 AM
更新人: