Hi,
We are developing a solution in which we need to enable CSEc strict mode.
When we do, by using the boot flavor '00' in the command CMD_BOOT_DEFINE, everything works fine.
However, after rebooting, if we update our boot loader and we try to define a new BOOT_SIZE, the command fails with code 0x800.
Even if we try to update with the same BOOT_SIZE, the command fails, no matter the Boot Flavor we use in the command. If we ignore the error and reboot, the part is bricked (even using the same BOOT_SIZE and updating the MAC appropriately).
The same process works without issue if the Sequential Boot Method is selected. The documentation states that Strict mode is OTP, but that BOOT_SIZE can be changed.
How can we update BOOT_SIZE in Strict mode?
Thank you very much!
Thank you very much for clarifying this.
Best regards,
Carlos
Hi @sinixtek
the result is that the SIZE cannot be updated. The sentence in the manual is confusing, I asked to update it.
Thanks for pointing this out.
Regards,
Lukas
Hi @lukaszadrapa ,
Thank you very much for your support, let's see what they say.
Best regards,
Carlos
Hi @sinixtek
That's a good question, I have never tried this use-case. It looks like you are the first one who is trying to change the BOOT_SIZE in strict boot mode. Please give me more time to clarify this. I will probably need to discuss this with another team, so it may take some time. At a glance, my guess is that it's not supported even if the documentation says something different. But let's wait for the result.
Regards,
Lukas