1947759_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1947759_en-US

1947759_en-US

can/canfd on GLDBOX

Hello,

        I want to use can/canfd on GLDBOX, now the GLDBOX software is as default, Linux on A core, and M core is not used.  I need some guide:

      1、Dose CAN/CANFD hardware resource designed for A core or M core or both?

     2、How to control CAN/CANFD from A core?

     3、Do I must install LLCE firmware before I use CAN/CANFD?





Re: can/canfd on GLDBOX

Hi, @yangjinzhuang 

Thanks for your post.

  1. The CAN peripherals could be used by both A&M cores.
  2. You may simple operation the corresponding interface under Linux according to the chapter12&13 BSPUM
  3. If you are willing to use the LLCE-CAN interface, then LLCE firmware is a must.

BR

Chenyin

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:53 PM
Updated by: