1947726_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1947726_en-US

1947726_en-US

CodeWarrior 2.1 and CodeWarrior 10.6 PE Driver

PE Driver(multilink_universal_install_12.2 ) can use on CodeWarrior 2.1 IDE ,but  it can not use on the CodeWarrior 10.7, it must instatll 12.7. Is PE Driver can used on the both CodeWarrior 2.1 IDE and CodeWarrior 10.7 IDE?

Re: CodeWarrior 2.1 and CodeWarrior 10.6 PE Driver

Hi,

Could you please help me to resolve this error.

ArunMukundan_0-1733385722303.pngArunMukundan_0-1733385722303.png


PFB is me driver details

ArunMukundan_1-1733385776134.pngArunMukundan_1-1733385776134.png


The USB indication led is turned on and it is blue color. 

Still the software is not detecting the hardware.

Re: CodeWarrior 2.1 and CodeWarrior 10.6 PE Driver

Thank you!

Re: CodeWarrior 2.1 and CodeWarrior 10.6 PE DriverIT is not found elf.file ,reload the elf file to the pathRe: CodeWarrior 2.1 and CodeWarrior 10.6 PE Driver

Hi 

ZhaoDinan_0-1728636156338.pngZhaoDinan_0-1728636156338.png

Thank you, I solved the PEmicro recognition problem using the method above, but now I'm encountering the "load fail" issue.

when I clicked the "connect(Reset)"button ,the new problem was appeared as below. And how can I solve this problem ?(load aborted)

ZhaoDinan_1-1728636195461.pngZhaoDinan_1-1728636195461.png


Re: CodeWarrior 2.1 and CodeWarrior 10.6 PE Driver

Thank you for your replying

Re: CodeWarrior 2.1 and CodeWarrior 10.6 PE Driver

Can you try to install P&E patch available here:

https://www.pemicro.com/downloads/download_file.cfm?download_id=463

This should update the support for all compatible PEmicro interfaces into CW MPC55xx/56xx v2.10

Stan

Re: CodeWarrior 2.1 and CodeWarrior 10.6 PE Driver

Hi,Thank you for your replying. My window is Windows 11 64bit , My drive and PE type is as following figure

Yorn_0-1725928745017.pngYorn_0-1725928745017.png 

Yorn_2-1725929907851.pngYorn_2-1725929907851.png

When debuging on  CodeWarrior 2.10 using multilink_universal_install _12.7. It is not ok,

Yorn_3-1725930239613.pngYorn_3-1725930239613.png

When debuging on  CodeWarrior 2.10 using multilink_universal_install _12.0. It is  ok,

Yorn_4-1725930353288.pngYorn_4-1725930353288.png




Re: CodeWarrior 2.1 and CodeWarrior 10.6 PE Driver

Hi, 

I've just installed Drivers 12_7 on my Windows 10 64bit machine and use it with CodeWarrior for MPC55xx/56xx v2.10 and

  • PEmicro Multilink FX (black probe) rev.C
  • PEmicro Multilink PowerPC Nexus (blue probe) rev.

stanish_0-1725886325651.pngstanish_0-1725886325651.png

All configurations work as expected.


Do you observe any issue on your side?

If yes, can you attach the error screenshot?

Hope it helps.

Stan

Re: CodeWarrior 2.1 and CodeWarrior 10.6 PE Driver

Hello,

@stanish could you comment here?

Best regards,

Peter

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 08:53 PM
更新者: