1946745_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1946745_en-US

1946745_en-US

S32G399A - Is Device Tree Configuration for U-Boot required?

Dear NXP fellows,


I see, for example, that in the Release BSP41.0 of U-Boot, there is no specific DTS or DTSI files concerning the S32G399A board in https://github.com/nxp-auto-linux/u-boot/tree/release/bsp41.0-2022.04/arch/arm/dts .

The Arm-Trusted Firmware has the DTS files for the S32G boards.

However, I saw one project where the developer patched U-boot for including the configurations required by the S32G boards.


So, my question is: Are the DTS configurations in this case managed exclusively by the ATF or I do have to manage the DTS in U-Boot too?


Thanks for your help,

Best regards,

Guilherme

Re: S32G399A - Is Device Tree Configuration for U-Boot required?

Hello @chenyin_h ,


Thank you very much for the answer!


Best regards,


Guilherme

Re: S32G399A - Is Device Tree Configuration for U-Boot required?

Hello, @GuilhermeS32G3 

Thanks for the post

From BSP's perspective, the dts is managed by ATF, you may not need to modify the files under u-boot.


BR

Chenyin

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:54 PM
Updated by: