1945802_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1945802_en-US

1945802_en-US

S32M244LC high-voltage detect threshold

Hi

     I have a question about high voltage threshold Settings,S32M244LC‘s GDU will be closed when VSUP over 22.6V,Where can I set this value(such as set to 28V),No description of this section is found in the RM &datasheet.

     thanks


Re: S32M244LC high-voltage detect threshold

hi Pavel,

   Thank you and regards,

Re: S32M244LC high-voltage detect threshold

Hi Yan,

there is a possibility to set bit HDHVDCFG to 1 , in GDU/CFG register (S32M24x RM rev2, page 1165).  With this bit set, thresholds VHVHDHA and VHVHDHD will be used for overvoltage detector. Thresholds VHVHDHA (min-typ-max: 30.65-32.5-34.6V) and VHVHDHD (min-typ-max: 29.65-31.5-33.6V) are defined in S32M2xx DS rev3, page 38/39

Best regards,

Pavel

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:56 PM
Updated by: