1945212_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1945212_en-US

1945212_en-US

S32K344-How to implement [detect one bit errors without correction]

Hello

I saw the description in the following figure in the file [S32K3xx Safety Manual]. How is [detect one bit errors without correction] implemented?


BestRegards,

Simon

Re: S32K344-How to implement [detect one bit errors without correction]

Yes, correct.

Re: S32K344-How to implement [detect one bit errors without correction]

Hi @davidtosenovjan 

So what this means is that the ECC for data is 1-bit correction. The ECC for address is 1-bit detection without correction?


BestRegards,

Simon

Re: S32K344-How to implement [detect one bit errors without correction]

In the RM, it is not explicitly defined which ECC SECDEC (single error correction, double error detection) variant is used, however it is clear that this code is capable to detect single bit error in the address.

Re: S32K344-How to implement [detect one bit errors without correction]

Hello

Sorry, here is the picture I mentioned before.

SimonLiu_0-1725410782093.png


Re: S32K344-How to implement [detect one bit errors without correction]

Could you point out which figure you have on your find?

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:56 PM
Updated by: