Mcl_Trgmux_GroupHi,
Mcl_Trigger Mux Group was there in that Group From TRGMUX_IP_INPUT_EMIOS1_IPP_ 0 to 15 ,22 and 23. If i want Select the Trgmux_Logic_trigger Hardware Input of emios channel to Hardware Out of Lcu0. currently Im using Emios Channel number 21,22. So which Trgmux Logic Trigger Input i need to select for channel num 21 and 22.

Re: Mcl_Trgmux_GroupHi @Senlent,
Thank u For Ur Quick Response towards the the Solution. It doesn't mean that NXP , It mean Each Emios Instance Have 24 Channels, So if U see the TRGMUX Connectivity 0 to 15,22,and 23 channels only in TRGMUX logic Group. If i use Emios Out of 23 channels why 16 to 21 channels Input not Available in that Option. .Re: Mcl_Trgmux_GroupHi@gadilinga
"But That Channel Suggested NXP only."
what does it mean? Can you show me a screenshot?
Re: Mcl_Trgmux_GroupHi @Senlent,
But That Channel Suggested NXP only.Re: Mcl_Trgmux_GroupHi@gadilinga
This is not a problem. eMIOS's CH21 cannot be used as the input of TRGMUX. What you can do is to change other channels.
Re: Mcl_Trgmux_GroupHi @Senlent,
Currently I'm using Emios0_Ch[0],Emios0_Ch[1], Emios1_Ch[6],Emios1_Ch[7],Emios1_Ch[21 And Emios1_Ch[22] these 6 channel using For Pwm.
i need Each channel Emios Input Trigger Mux AS for NXP Application:AN13767 :S32K344 module interconnection Diagrams. for Got 5 channels But 21 I didn't get So As u mention Above comment. what was Solution for This Problem.Re: Mcl_Trgmux_GroupHi@gadilinga
Actually you can see what channel can be used in TRGMUX.
Senlent_0-1725007983445.png
and EMIOS_0_IPP_DO_eMIOS_CH[21] can not be used for TRGMUX input.