1943260_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1943260_en-US

1943260_en-US

s32g3 VR5510 standby mode entry

Hi,

I am trying to control the VR5510 into standby mode, my base project is the RTD4.0 example ‘Pmic_Configuration_Autosar_Example_S32G399A_M7’

jiajun_0-1724918543800.png

My revision points are the following:

1. Modify the target mode of the structure Pmic_VR55XX_ModeConfigPB_0_0,base value is PMIC_NORMAL_MODE(Is it possible to change only the target mode?)

jiajun_2-1724918752246.png

2. Modify the power mode name of the structure Power_Ip_aModeConfigPB,base value is POWER_IP_RUN_MODE

jiajun_4-1724918946739.png

3. Modify the I2C address to 0x21

jiajun_5-1724919465621.png


4. Add the following code to the main function,write 0x20 to address 0x19,use Pmic_SetMode and Power_Ip_SetMode

This post referenced:https://community.nxp.com/t5/Power-Management/VR5510-Standby-mode-entry/m-p/1536237

jiajun_1-1724918687575.png

Finally, use the S32 Debug Probe to simulate

Am I going into Standby the right way please?

note:Before adding the command sent by I2C, running the program will keep starting again and again, after adding it it doesn't happen, how should I test that the chip is in standby mode

My environments:

S32G-VNP-RBD3, S32DS 3.5 ,RTD4.0

VR5510 S32G-VNP-RDB3 

Re: s32g3 VR5510 standby mode entry

Hello, @chenyin_h :
    I see that there is a section about entering and exiting Standby in the S32G3 RM documentation. So if I enter Standby, do I need to configure not only VR5510 but also S32G3?Is there any simple example for me to refer to?

Re: s32g3 VR5510 standby mode entry

Hello, @jiajun 

Thanks for the post and sorry for the delay.

From my opinion, your modification may not be enough, since some hardware configurations must be done before entering Standby mode. you may reference the AN12880 for details.

For standby mode, maybe the following information is useful for your detailed reference.

https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/nxp-designs%40tkb/700/1/S32G_Standby_Dem...

I hope it will help.


BR

Chenyin

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 11:55 AM
更新者: