I do not understand the purpose of the ADC I and Q channels on the PN512. PN512 provides a way of reading the value by reading register 0x3b but I don't understand what the values I am getting are supposed to represent.
With the Field turned off I get a value of 0x88.
With the Field turned on I get a value of 0xf0, sometimes 0xff.
If someone could provide an explanation, that would be great.
Thank You
Hi,
ADC_I and ADC_Q, both are just ADC sampling values, indicating the variation of a noise into RX. For a device featuring LPCD functionality, please consider our latest focus products from our NFC Readers portfolio.
Regards,
Eduardo.
Thank you for your reply,
To follow up, when I am reading register 0x3B what do the values in that register represent? Voltage? Current?
The PN512 document simply describes it as "the actual value of ADC I/Q channel". What kind of value is it?
Is there a way to use that value to detect the presence of a tag?
Thank You
Hello @user_leo,
Hope you are doing well.
I and Q are part of the RX section of the device:
These two signals could be taken to judge the overall RX signal quality. You can see an example of ADC I channel behavior in AN11038 Fast Verification of PN512 and amplifier, Section 3.1.1.
Regards,
Eduardo.