1938124_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1938124_en-US

1938124_en-US

RT1020 EVK , SDK wi-fi direct support is possible?

Hello , 

It is simple question, 

I reviewd all  example about wifi.   but

I Can not find  the example of wi-fi direct funtionality   in  SDK 2.13.0 RT1020.

So. Is there  any doc. or someting  about Entering wi-fi direct mode from Station mode?

Do I have to  implement wi-fi direct using  Soft AP  of   wifi_cli example

i.MXRT 102xRe: RT1020 EVK , SDK wi-fi direct support is possible?

Hi @Seongyon_Jeong 

It seems difficult to implement wifi direct feature base on RT1020 EVK board, the root causes are SW resouce limitation and adapation of some modules of M.2 interface, so we can find the SDK/example in RT1050/1060/11xx, but we can not support them in RT1020 EVK. 

Sorry for inconvenient.


B.R,

Sam

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 04:35 PM
Updated by: