Hi , Im testing Icu Module Example code in S32K344 Code was Working But My query is In peripheral Icu Module configuration User_edge dection(); function Is there But its not triggering that function then why that function used in that Example code can i Know the reason. i download the training Document also mention. i didn't understand. thank u
Test the project in SIUL2 external interrupt example project using S32K3 RTD without AUTOSAR. SIUL2 eirq13(SW4 PTB26) is configured for ICU_RISING_EDGE. When you press SW4 to generate a rising edge, it should enter it's own IcuSignalNotification(for example: SW4_eirq13_PTB26_Callback )
In addition, when debugging, you can also set a breakpoint in Siul2_Icu_Ip_ProcessInterrupt (RTD/src/Siul2_Icu_Ip_Irq.c) and observe which EIF bit of the 10.6.4 SIUL2 DMA/Interrupt Status Flag 0 (DISR0) register was set.
Did you read the link I gave you? I think if you refer to it and - S32K3xx Pins and Clocks with RTD - Training, you should be able to implement SIUL2 external interrupt according to the pin EIRQ number you modified.
I don't understand your question. Please tell me which pin do you need to set as EIRQ to trigger the interrupt?
Hi
I don't know which training you are watching, so I'm not sure if the content is complete.
Please tell me the link of the training.
I also recommend you refer to: SIUL2 external interrupt example project using S32K3 RTD without AUTOSAR
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------