1936233_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1936233_en-US

1936233_en-US

Urgent - Driver NXP Pegoda CL RD701

Hello,


I need the driver for the NXP Pegoda CL RD701 (Windows 11) to use it in RFIDDiscover :

https://www.nxp.com/products/rfid-nfc/mifare-hf/mifare-desfire/rfiddiscover:RFID-DISCOVER

(RFIDDiscover compatible reader)

I need this driver asap to encode NXP NTAG 424 DNA chips. I have already tried with the TagXplorer software and the Identiv uTrust 3700 F reader. The software is no longer up to date and so it didn't work. I really need to encode my chips asap so please provide me with the drivers for the NXP Pegoda CL RD701 reader which are not on the site.


Best regards

Re: Urgent - Driver NXP Pegoda CL RD701

Hi guys, can somebody please send me also driver for NXP Pegoda RD 701? Thanks you a lot

Re: Urgent - Driver NXP Pegoda CL RD701

hi @danielchen , Would you please send me win10x64 driver of rd 701? Thanks!

Re: Urgent - Driver NXP Pegoda CL RD701

@binhdao ;  ok, will send to you later today.  please create a support account first using blow link ,    https://www.nxp.com/webapp-signup/register?referrerUrl=https://www.nxp.com/products/power-management...

I will send it to your account.

Re: Urgent - Driver NXP Pegoda CL RD701

hi @danielchen , could you send me the dirver of rd 701?


Thanks,


Binh

Re: Urgent - Driver NXP Pegoda CL RD701

please mail me zhe RD701 driver for windows 7  x64,thank you!

Re: Urgent - Driver NXP Pegoda CL RD701Hi Daniel,

I'm in the same case as Loick, I want to use my old NXP Cl RD 701 Pegoda under Windows 10. Could you send me the Windows 7 driver. Thanks.

Charles
Re: Urgent - Driver NXP Pegoda CL RD701

Hi @Loick :


Please check my attached driver, it is for win 7,  and should work on your win10.


Regards

Daniel

Re: Urgent - Driver NXP Pegoda CL RD701

Hi Daniel,

Thank you for your prompt response.

I’m a bit puzzled as to why the CLRD 701 is listed as a compatible reader for RFIDDiscover if it is indeed very old and no longer maintained. The NTAG 424 DNA chips are relatively recent (2019) and use the advanced DNA technology, so it’s surprising that an outdated reader would be recommended for encoding these.

Is there at least a driver available for Windows 10 if there isn't one for Windows 11? Given that Windows 2000 had its last update in 2005, I highly doubt that we would be able to install RFIDDiscover and successfully encode NTAG 424 DNA chips on such an old system.

If possible, could you please send us (by email ok) any available drivers for the NXP Pegoda CL RD701 so we can test them as soon as possible? Also, the reader you suggested (CLRD730) is currently out of stock on the website. We urgently need a solution for encoding NTAG 424 DNA chips that includes both a compatible reader and software.

Could you advise on the fastest way to set this up?

Best regards,
Loïck

Re: Urgent - Driver NXP Pegoda CL RD701

Hi Loick:


CLRD 701 is very old, and not maintained any more.  so you can not find it on the site

I would suggest you use CLRD730, please refer to below link for more details.

PEGODA Contactless Smart Card Reader | NXP Semiconductors


There is no CLRD 701 driver for windows 11, only have a driver for windows 2000.

If I can find it on my old pc, and you still need it, I will send it to you via email tomorrow morning .


Regards

Daniel

Re: Urgent - Driver NXP Pegoda CL RD701hi daniel. could you please send me the driver of CL RD701 for win10 as well. i have a device in production, which is not working. i need it to reinstall the driver.Thank youRe: Urgent - Driver NXP Pegoda CL RD701Hi, Chuck, could you please share the driver with me as well? for CL RD701 used in window10. Thank you!
Tags (1)
No ratings
Version history
Last update:
18 hours ago
Updated by: