1926087_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1926087_en-US

1926087_en-US

P3T1035XUK-ARD/MIMXRT685-EVK MCU

P3T1035XUK-ARD evaluation board connecting to the MIMXRT685-EVK MCU board. Where can I download the firmware for MIMXRT685 running P3T1035XUK-ARD.thinks

Re: P3T1035XUK-ARD/MIMXRT685-EVK MCU

ok. The problem has been resolved. 

Use J-Link LPCXPresso(J-Link Commander) to program MIMXRT685. Start Addr= 0x08000000

Re: P3T1035XUK-ARD/MIMXRT685-EVK MCU

Hello,Tomas

May I inquire about the burning issue: What is the starting address of the bin file? 0x08000400? Using J-Link to download, is it connected to J2's pin2, pin4, pin10, and gnd? Is it powered by J7? According to this, it cannot be connected to the IC,Or is there any other GUI that can burn bin files through J5? thanks



Re: P3T1035XUK-ARD/MIMXRT685-EVK MCU

Thank you very much.

Re: P3T1035XUK-ARD/MIMXRT685-EVK MCU

Hello Zhang,

Please find attached the FW .bin file for MIMXRT685-EVK MCU board to run with P3T1035XUK-ARD GUI.

BRs, Tomas

Re: P3T1035XUK-ARD/MIMXRT685-EVK MCUOkay, thank you very much. Looking forward to your updates!Re: P3T1035XUK-ARD/MIMXRT685-EVK MCU

Okay, thank you very much. Looking forward to your updates!

Re: P3T1035XUK-ARD/MIMXRT685-EVK MCU

Hello Zhang,

I also was not able to find the required firmware on the product webpage, so I have asked the developer of this board to share it if possible. I will update this thread as soon as I have his feedback.

BRs, Tomas

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 09:13 PM
更新者: