1917108_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1917108_en-US

1917108_en-US

Does the 55 pin of the LPC55S28 have PWM capability?

At present, I need three PWM signals to control RGB LED. The 53, 55 and 58 pins of LPC55S28 have been selected as the PWM output signal pins. Is this method feasible?

Re: Does the 55 pin of the LPC55S28 have PWM capability?

Hi JJ3 

No, other two 53 pin (CTIMER0_MATCH1) and 58 pin (CTIMER0_MATCH2) will not affect the GPIO output of 55 pins.

Hope this helps,

Jun Zhang

Re: Does the 55 pin of the LPC55S28 have PWM capability?Hi Jun,
Now I'm trying to turn on at pin 60 (CTIMER0_MATCH0) as a PWM signal and then sync with GPIO output at pin 55 so I can use three PWM channels at the same time. Will the other two 53 pins (CTIMER0_MATCH1) and 58 pins (CTIMER0_MATCH2) affect the GPIO output of 55 pins? Here's my code for that


void ctimer0_init(void)
{
ctimer_config_t config;
uint32_t srcClock_Hz;
CLOCK_AttachClk(kFRO_HF_to_CTIMER0);

srcClock_Hz = CTIMER0_CLK_FREQ;
CTIMER_GetDefaultConfig(&config);
timerClock = srcClock_Hz / (config.prescale + 1);

CTIMER_Init(CTIMER0, &config);

CTIMER_RegisterCallBack(CTIMER0, &ctimer_callback[0], kCTIMER_SingleCallback); //kCTIMER_MultipleCallback kCTIMER_SingleCallback
/* Get the PWM period match value and pulse width match value of 2Khz PWM signal */
CTIMER_GetPwmPeriodValue(PWM_FRQ, dutyCycle, timerClock);
CTIMER_SetupPwmPeriod(CTIMER0, CTIMER0_MAT0_PWM_PERIOD_CHANNEL, CTIMER0_MAT0_OUT, g_pwmPeriod, g_pulsePeriod, true);
CTIMER_SetupPwmPeriod(CTIMER0, CTIMER0_MAT0_PWM_PERIOD_CHANNEL, CTIMER0_MAT1_OUT, g_pwmPeriod, g_pulsePeriod, true);
CTIMER_SetupPwmPeriod(CTIMER0, CTIMER0_MAT0_PWM_PERIOD_CHANNEL, CTIMER0_MAT2_OUT, g_pwmPeriod, g_pulsePeriod, true);
pwm_set_duty(global_bright_rgb);
CTIMER_StartTimer(CTIMER0);
}
if (CTIMER_GetOutputMatchStatus(CTIMER0, CTIMER0_MAT0_OUT))
{
bsp_led_off(LED_B);
}
else
{
bsp_led_on(LED_B);
}
void pwm_match_callback(uint32_t flags)
{
(void) flags;
if (times_ms >0)
{
times_ms--;
}
}

Thanks!
Re: Does the 55 pin of the LPC55S28 have PWM capability?

Hello JJ3 ,

Yes. you can use  53PIN (ctimer0_match1) to output to a spare GPIO. then set 55PIN as GPIO to synchronize 53PIN output.

Hope this can help you,

Jun Zhang

Re: Does the 55 pin of the LPC55S28 have PWM capability?Hi,Jun
Now our PCBA has been completed. Can we control 55PIN by using 53PIN (ctimer0_match1) and simulate output PWM waveform through GPIO output?Is there any other way to do PWM control without changing the hardware?
Thanks!
Re: Does the 55 pin of the LPC55S28 have PWM capability?

Hello JJ3 

Pin 53 and 58 can be used as PWM output pin but Pin55 can be only set as input. see below extacted from DS. If we need PWM output, we need to choose another pin which can support PWM output.

ZhangJennie_1-1722247020367.png


Hope this will help you,

Jun Zhang


Re: Does the 55 pin of the LPC55S28 have PWM capability?Hi Jun,
I use the mcu package of LPC55S28JBD64.
Thanks!
Re: Does the 55 pin of the LPC55S28 have PWM capability?

Hello @JJ3 

Could you let me know your part package?

Thanks,

Jun Zhang

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 12:52 PM
更新者: