The current underlying implementation of the textarea treats the text as a complete label. Modifying its color is applicable to the whole text, but cannot meet some practical scenarios. For example, if it is embedded in the host computer of some industrial computers and the entire edited text has only one color, the interface cannot be user-friendly. As for span, although it has multiple labels, it does not meet the functions of online real-time editing and interaction of text. Is it under development or is there a plan for this? Or is there an internal test version that can realize this function?