1906311_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1906311_en-US

1906311_en-US

LS1043a and LS1046a botting from QSPI MRAM

Hello,

I am working on a custom board that will use either the LS1043A or the LS1046A, exactly which processor is TBD and I need some clarification on QSPI-boot hardware requirements.

The current thinking is to boot from QSPI using a non-volatile serial MRAM module.


My questions are:


1) Can I boot from a serial MRAM module connected to QSPI? Or does it have to be flash for QSPI-boot?

2) If I use the QSPI interface to boot but I set the RCW values in the PBI such that the QSPI interface is not used during normal operation, will I be able to use all IFC pins as IFC pins? Or, if I boot from QSPI are those pins permanently muxxed to QSPI during normal operation?

3) If it's possible to boot from QSPI using MRAM, are there any special procedures we need to follow in code to make that work?


Thank you 

Re: LS1043a and LS1046a botting from QSPI MRAM

Hello,

Q1) Flash is recommended as boot-source.

Q2)Once you set the pins in the RCW you cannot change the mux without updating the RCW and re-boot.

Q3)It should be possible, not recommended as boot source and it only have to meet the requirements for the QSPI boot in the RM.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 09:31 PM
更新者: