Hello,
ここでは、XIP で実行される 64 MB の外部フラッシュと 64 MB の SDRAM を搭載した MIMXRT1176 を使用しています。
SDRAM の最後の 16 MB をキャッシュ不可にしたいと考えています。ただし、SDK のデフォルトの MPU コンフィギュレーションを見ると、M7 コアのすべての領域 (0 から 15) が取得されます (以下のスニペット)。これらのメモリ領域については、リファレンスマニュアルを見て回ったところ、ほとんどが予約済み/使用中です。
アドレス 0x8300_0000 に 16 MB のキャッシュ不可能な領域のためのスペースを確保するために、安全にあきらめることができる領域 (またはその他のアイデア) はありますか?
SDRAM アドレス空間を合計 3 つの領域から再構築する必要があります。
リージョン 2 (FlexSPI2、0x6000_0000) は使用していないため (XIP フラッシュは FlexSPI1 にあります)、安全に再利用できると考えていますが、それはまだもう 1 つのリージョンが不足していることを意味します。
助けてくれてありがとう!
/* MPU configuration. */
#if __CORTEX_M == 7
void BOARD_ConfigMPU(void)
{
/* ... some variable definitions ... */
#if defined(__ICACHE_PRESENT) && __ICACHE_PRESENT
/* Disable I cache and D cache */
if (SCB_CCR_IC_Msk == (SCB_CCR_IC_Msk & SCB->CCR))
{
SCB_DisableICache();
}
#endif
#if defined(__DCACHE_PRESENT) && __DCACHE_PRESENT
if (SCB_CCR_DC_Msk == (SCB_CCR_DC_Msk & SCB->CCR))
{
SCB_DisableDCache();
}
#endif
/* Disable MPU */
ARM_MPU_Disable();
/* MPU configure:
* Use ARM_MPU_RASR(DisableExec, AccessPermission, TypeExtField, IsShareable, IsCacheable, IsBufferable,
* SubRegionDisable, Size)
* API in mpu_armv7.h.
* param DisableExec Instruction access (XN) disable bit,0=instruction fetches enabled, 1=instruction fetches
* disabled.
* param AccessPermission Data access permissions, allows you to configure read/write access for User and
* Privileged mode.
* Use MACROS defined in mpu_armv7.h:
* ARM_MPU_AP_NONE/ARM_MPU_AP_PRIV/ARM_MPU_AP_URO/ARM_MPU_AP_FULL/ARM_MPU_AP_PRO/ARM_MPU_AP_RO
* Combine TypeExtField/IsShareable/IsCacheable/IsBufferable to configure MPU memory access attributes.
* TypeExtField IsShareable IsCacheable IsBufferable Memory Attribute Shareability Cache
* 0 x 0 0 Strongly Ordered shareable
* 0 x 0 1 Device shareable
* 0 0 1 0 Normal not shareable Outer and inner write
* through no write allocate
* 0 0 1 1 Normal not shareable Outer and inner write
* back no write allocate
* 0 1 1 0 Normal shareable Outer and inner write
* through no write allocate
* 0 1 1 1 Normal shareable Outer and inner write
* back no write allocate
* 1 0 0 0 Normal not shareable outer and inner
* noncache
* 1 1 0 0 Normal shareable outer and inner
* noncache
* 1 0 1 1 Normal not shareable outer and inner write
* back write/read acllocate
* 1 1 1 1 Normal shareable outer and inner write
* back write/read acllocate
* 2 x 0 0 Device not shareable
* Above are normal use settings, if your want to see more details or want to config different inner/outter cache
* policy.
* please refer to Table 4-55 /4-56 in arm cortex-M7 generic user guide
* param SubRegionDisable Sub-region disable field. 0=sub-region is enabled, 1=sub-region is disabled.
* param Size Region size of the region to be configured. use ARM_MPU_REGION_SIZE_xxx MACRO in
* mpu_armv7.h.
*/
/*
* Add default region to deny access to whole address space to workaround speculative prefetch.
* Refer to Arm errata 1013783-B for more details.
*
*/
/* Region 0 setting: Instruction access disabled, No data access permission. */
MPU->RBAR = ARM_MPU_RBAR(0, 0x00000000U);
MPU->RASR = ARM_MPU_RASR(1, ARM_MPU_AP_NONE, 0, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_4GB);
/* Region 1 setting: Memory with Device type, not shareable, non-cacheable. */
MPU->RBAR = ARM_MPU_RBAR(1, 0x80000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_512MB);
/* Region 2 setting: Memory with Device type, not shareable, non-cacheable. */
MPU->RBAR = ARM_MPU_RBAR(2, 0x60000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_512MB);
/* Region 3 setting: Memory with Device type, not shareable, non-cacheable. */
MPU->RBAR = ARM_MPU_RBAR(3, 0x00000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_1GB);
/* Region 4 setting: Memory with Normal type, not shareable, outer/inner write back */
MPU->RBAR = ARM_MPU_RBAR(4, 0x00000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_256KB);
/* Region 5 setting: Memory with Normal type, not shareable, outer/inner write back */
MPU->RBAR = ARM_MPU_RBAR(5, 0x20000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_256KB);
#if defined(CACHE_MODE_WRITE_THROUGH) && CACHE_MODE_WRITE_THROUGH
/* Region 6 setting: Memory with Normal type, not shareable, write through */
MPU->RBAR = ARM_MPU_RBAR(6, 0x20200000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 0, 0, ARM_MPU_REGION_SIZE_1MB);
/* Region 7 setting: Memory with Normal type, not shareable, write trough */
MPU->RBAR = ARM_MPU_RBAR(7, 0x20300000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 0, 0, ARM_MPU_REGION_SIZE_512KB);
#else
/* Region 6 setting: Memory with Normal type, not shareable, outer/inner write back */
MPU->RBAR = ARM_MPU_RBAR(6, 0x20200000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_1MB);
/* Region 7 setting: Memory with Normal type, not shareable, outer/inner write back */
MPU->RBAR = ARM_MPU_RBAR(7, 0x20300000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_512KB);
#endif
#if defined(XIP_EXTERNAL_FLASH) && (XIP_EXTERNAL_FLASH == 1)
/* Region 8 setting: Memory with Normal type, not shareable, outer/inner write back. */
MPU->RBAR = ARM_MPU_RBAR(8, 0x30000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_64MB);
#endif
#ifdef USE_SDRAM
#if defined(CACHE_MODE_WRITE_THROUGH) && CACHE_MODE_WRITE_THROUGH
/* Region 9 setting: Memory with Normal type, not shareable, write trough */
MPU->RBAR = ARM_MPU_RBAR(9, 0x80000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 0, 0, ARM_MPU_REGION_SIZE_64MB);
#else
/* Region 9 setting: Memory with Normal type, not shareable, outer/inner write back */
MPU->RBAR = ARM_MPU_RBAR(9, 0x80000000U);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 0, 0, 1, 1, 0, ARM_MPU_REGION_SIZE_64MB);
#endif
#endif
while ((size >> i) > 0x1U)
{
i++;
}
if (i != 0)
{
/* The MPU region size should be 2^N, 5<=N<=32, region base should be multiples of size. */
assert(!(nonCacheStart % size));
assert(size == (uint32_t)(1 << i));
assert(i >= 5);
/* Region 10 setting: Memory with Normal type, not shareable, non-cacheable */
MPU->RBAR = ARM_MPU_RBAR(10, nonCacheStart);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 1, 0, 0, 0, 0, i - 1);
}
/* Region 11 setting: Memory with Device type, not shareable, non-cacheable */
MPU->RBAR = ARM_MPU_RBAR(11, 0x40000000);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_16MB);
/* Region 12 setting: Memory with Device type, not shareable, non-cacheable */
MPU->RBAR = ARM_MPU_RBAR(12, 0x41000000);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_2MB);
/* Region 13 setting: Memory with Device type, not shareable, non-cacheable */
MPU->RBAR = ARM_MPU_RBAR(13, 0x41400000);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_1MB);
/* Region 14 setting: Memory with Device type, not shareable, non-cacheable */
MPU->RBAR = ARM_MPU_RBAR(14, 0x41800000);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_2MB);
/* Region 15 setting: Memory with Device type, not shareable, non-cacheable */
MPU->RBAR = ARM_MPU_RBAR(15, 0x42000000);
MPU->RASR = ARM_MPU_RASR(0, ARM_MPU_AP_FULL, 2, 0, 0, 0, 0, ARM_MPU_REGION_SIZE_1MB);
/* Enable MPU */
ARM_MPU_Enable(MPU_CTRL_PRIVDEFENA_Msk);
/* Enable I cache and D cache */
#if defined(__DCACHE_PRESENT) && __DCACHE_PRESENT
SCB_EnableDCache();
#endif
#if defined(__ICACHE_PRESENT) && __ICACHE_PRESENT
SCB_EnableICache();
#endif
} VScode の場合、リンカを変更して他の SDRAM パーティションを持つ必要があります。MPUでncache領域を構成するには、添付されているコードを参照できます。
Omar_Anguiano_0-1721074971305.png
そこでは、SDRAM 領域は非キャッシュとして構成されています。リンカーは、この領域の開始位置を定義します。MCUXpressoを使用すると、MCU設定を変更できますが、VScodeを使用するとリンカを変更する必要があります。
Omar_Anguiano_1-1721075276067.png
よろしくお願いいたします
オマル
MCUの設定では、SDRAMのパーティションを作成できるため、MPUでは非キャッシュ設定を行います。
この 1 つの例は、EVK SDRAM の 1 つの領域が非キャッシュに設定されているため、一部の SDK の例にあります。
よろしくお願いいたします
オマル