1901601_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1901601_en-US

1901601_en-US

S32K344-If the DERR_SUP field is set to 1, will a single-bit error be repaired?

Hello

I read in the chip manual that if the DERR_SUP field in register PFCR4 is set to 1, single-bit and double-bit ECC events will not be reported. Will single-bit errors be repaired?


BestRegards,

Simon

Re: S32K344-If the DERR_SUP field is set to 1, will a single-bit error be repaired?

Yes, it has nothing to do with a single-bit ECC.


Regards,

Daniel

Re: S32K344-If the DERR_SUP field is set to 1, will a single-bit error be repaired?

Hello @danielmartynek 

Thank you for your answer. I have a similar question: If the DMEEE bit in the same register PFCR4 is set, will a single-bit error be repaired?


BestRegards,

Simon

Re: S32K344-If the DERR_SUP field is set to 1, will a single-bit error be repaired?

Hi @Simon-Liu,

Single bit errors are still corrected.


Regards,

Daniel

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 09:34 PM
更新者: