1901519_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1901519_en-US

1901519_en-US

SJA1110 SDK installation

Hi I want to install SJA1110 RTD SDK. i've installed S32DS FOR S32 PLATFORM V3.5.12, I have downloaded and installed SW32G_SJA11XX_ETH_SWITCH_4.4_1.0.0_DS_updatesite_D2306.zip, SW32SJA1110_XJA11XX_ETH_PHY_4.4_1.0.5_DS_updatesite_D2405.zip, SJA11XX_RTD_4.4_1.0.1_P01_D2404_DS_updatesite.zip, SJA11XX_RTD_4.4_1.0.1_D2312_DS_updatesite.zip, SJA11XX_ETH_SWITCH_4.4_1.0.0_DS_updatesite_D2306.zip, but I still can't find the ‘switch_config_s32g_vnp_rdb’ examples in

Re: SJA1110 SDK installation

Hi,

I struggled using the SDK because some (outdated?) documents told me it should show up in the S32 Design Studio for S32 Platform Help -> S32 DS Extensions and Updates list.
This is NOT the case. I needed to install the S32 SDK via file extraction of the .zip and then Help -> Install new software ... -> "Add..." and then "Local...". I did not try "Archive..." and .zip selection, may be this works also.

Best regards

Re: SJA1110 SDK installation

Hi, 

this example is within SJA1110 SDK, can be downloaded from https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SWSJA1110-SDK01E, latest version is S32 SDK for SJA1110 RTM 1.0.2. Download update zip package and add it to your S32DS. Read package release note document for the info about installation.

BR, Petr

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 09:35 PM
更新者: