This is my first attempt with MIMXRT1060-EVKB. I tried to run the example "helo word" and I could not upload the program. J-Link and CMSIS-DAP do not connect to MIMXRT1060-EVKB either. I do not know what to do next. Please help me what I can do.
Thanks for the quick response. A little effort and I solved the problem. Everything was in the article "Using J-Link with MIMXRT1060-EVKB or MIMXRT1040-EVK"
https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-J-Link-with-MIMXRT1060-EVKB-or-MIMXRT1040-...
J-Link works ok.
Ryszard
Hi @Ryszard
Are you using the MCUXpresso IDE?
If you use it.
You can download the SDK_2_15_100_MIMXRT1060-EVKB SDK on the NXP official site.
Select Board | MCUXpresso SDK Builder (nxp.com)
And import the downloaded SDK in MCUXpresso.
And import the example in SDK.
And click the debug to run the hello world.
Hope this will help you.
BR
Hang