Hello,
I am using S32DS pin tools to configure GMAC0, PFE0/1/2 interfaces. However, I am encountering numerous pin conflicts between GMAC0 and PFE1, as well as between PFE0 and PFE2. According to the "S32G-VNP-RDB3 Ethernet Enablement Guide," it seems that all four interfaces are able to be configured simultaneously, and supports multiple combinations. The dts/dtsi patch files do not provide sufficient information regarding the pin assignments when attempting to use all four interfaces together.
My questions are as follows:
Thank you for your assistance.
XD
Hello, @XD
Thanks for the update.
Yes, the PFE0 and PFE2 could be used simultaneously. Because on RDB3 with the BSP, the PFE0 is working on SGMII mode by default, the pins you listed are not actually used by PFE0, but by PFE2, so that no pin conflicts existed from my understanding.
Best Regards
Chenyin
Hi Chenyin,
I appreciate your support, and the files you provided are very helpful. According to the S32g.dtsi file, I noticed that PFE0 and PFE2 are using almost the same pin groups. Below are the PFE0/2 TX pin groups I found:
pfe0_pins: pfe0 {
pfe0_grp0 {
pinmux = ,
,
,
,
;
output-enable;
slew-rate = ;
}; pfe2_pins: pfe2 {
pfe2_grp0 {
pinmux = ,
,
,
,
;
output-enable;
slew-rate = ;
}; Given this overlap, could you please clarify how we can use PFE0 and PFE2 simultaneously?
Thank you for your assistance.
XD
Hello, @XD
It is my pleasure to support.
You may reference the dts file in TF-A’s source code, under fdts/, with the name s32xxx.dts/dtsi
Hope it helps
Best Regards
Chenyin
Hi Chenyin,
Thank you for your quick response. Regarding item 2, are the files in the kernel source code? Could you please point me to the DTS file name or the folder name of TF-A?
Thanks,
XD
Hello, @XD
Thanks for the questions.
Best Regards
Chenyin