1891676_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1891676_en-US

1891676_en-US

Installing new SDK causes automation project migration

I have S32 DS 3.5 and S32K344 micro.

It was originally set with SDK/RTD V2.0.0

It became necessary to add SDK 4.0.0, so that one project would migrate to 4.0.0 and another project stays at 2.0.0

SDK 4.0.0 gets installed properly and both SDKs appear under project settings.

I was expecting that by attaching/detaching SDK I can control which SDK current project would use.

However those "attached/detached" check-boxes seems to have no effect.

Regardless of that all projects would use 4.0.0 and it is was not possible to keep one project with 2.0.0

Is there a way to avoid that?

Re: Installing new SDK causes automation project migration

That works, thank you

Re: Installing new SDK causes automation project migration

Hi @sstelmak 

S32DS 3.5 can keep one RTD version only (plus additional extensions packages/stacks).

The solution is to install more S32DS instances. Just use different folder name of S32DS like:

c:\NXP\S32DS.3.5_RTD_200\

c:\NXP\S32DS.3.5_RTD_400\

And install corresponding RTD package to those instances.

Regards,

Lukas

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 04:54 PM
Updated by: