1890417_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1890417_en-US

1890417_en-US

difference between GoldVIP Real-time Gateway application image (Slot A) (Slot B)

Hello , 
I was going through the Gold VIP user manual "GoldVIP-S32G3-1.11.0-User-Manual.pdf",

Here i dnt understand the significance of GoldVIP Real-time Bootloader image (Slot A) (Slot B),or GoldVIP Real-time Gateway application image (Slot A) (Slot B).

what are these different slots , i can see when this software is flashed to Nor flash it will be using Slot A in both the case . 
I don't see anywhere the slot 2 is used what is the exact use case of this slot 2


Karthik_7_0-1718802093923.png

Regards

Karthik Mallya M


GoldVIPRe: difference between GoldVIP Real-time Gateway application image (Slot A) (Slot B)

Hello @Bio_TICFSL 
Thank you for the response ,
To be clear my quetion is in current GoldVIP-S32G3-1.11.0 package ,is this space is in use or not ?, because even we will not load any application to this area while flashing  we are using only Slot A 
i am asking becasue i am planning to use this area for other memory allocation like NvM area, before doing that i wanted to confirm


Regards

Karthik 

Re: difference between GoldVIP Real-time Gateway application image (Slot A) (Slot B)

Hello,

There is no linker because we have no any example of it, but you can modify current linker file and add a memory through QSPI or a sensor, etc.

Regards

Re: difference between GoldVIP Real-time Gateway application image (Slot A) (Slot B)

Hello @Bio_TICFSL ,

Could you Brief me what kind of application ,because I don't see any linker assignment for these slot

Re: difference between GoldVIP Real-time Gateway application image (Slot A) (Slot B)

Hello,

The SLOT B it uses for application.

Regards

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 11:06 PM
Updated by: