1887045_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1887045_en-US

1887045_en-US

how to start with clock_ip_ReferencePoints

In S32k358, how can I use  already defined clk ?

Thanks!


jimmy623_0-1718285913351.png


Re: how to start with clock_ip_ReferencePoints

Hello @jimmy623,

I see, it is a bug in RTD 3.0.0, it has been fixed in RTD 4.0.0


Regards,

Daniel

Re: how to start with clock_ip_ReferencePoints

I will check RTD 4.0 later


jimmy623_0-1718767373703.pngjimmy623_1-1718767416221.png

jimmy623_2-1718767633620.png



Re: how to start with clock_ip_ReferencePoints

That is the Autosar version, I mean RTD version.

For example, in this version, it is correct:

danielmartynek_0-1718705944216.png

danielmartynek_1-1718705969722.png


Regards,

Daniel



Re: how to start with clock_ip_ReferencePoints

Which RTD version is it?


Thank you.

Re: how to start with clock_ip_ReferencePoints

This is a Bug?


jimmy623_1-1718693326375.png


jimmy623_0-1718693247334.png


Re: how to start with clock_ip_ReferencePoints

Hello @jimmy623,

The LPUART modules are clocked either by AIPS_PLAT_CLK or AIPS_SLOW_CLK depending on the number of the instance, this cannot be changed. Refer to the RM.

danielmartynek_0-1718692142774.png


Regards,

Daniel

Re: how to start with clock_ip_ReferencePoints

How can i use to LPUART driver ?

default Baud rate is 40M ,which mismatch to Reference design.

Thanks!

jimmy623_0-1718674157426.png

jimmy623_1-1718674289966.png


Re: how to start with clock_ip_ReferencePoints

Hello @jimmy623,

The references can be used by other RTD drivers.

Such as BaseNXP Osif Config, see below.

There is no list of drivers dependent on the clock reference points.

danielmartynek_0-1718354112906.png


Regards,

Daniel


Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 01:53 PM
Updated by: