1886169_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1886169_en-US

1886169_en-US

Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the
 UART IP Driver for the S32K3xx MCU.

 The example uses LPUART6 for transmit & receive five bytes using the DMA.


 ------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-T172
* MCU: S32K344
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

Dinesh_Guleria_0-1718197381145.pngDinesh_Guleria_0-1718197381145.png



Dinesh_Guleria_1-1718197381161.pngDinesh_Guleria_1-1718197381161.png

Putty output :--

Dinesh_Guleria_2-1718197434242.pngDinesh_Guleria_2-1718197434242.png
Re: Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300

Hi @Dinesh_Guleria ,


Can we use DMA without Autosar (RM CDD)? 

Re: Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300

@Dinesh_Guleria  do you have an example of DMA UART in RTD 4.0.0?

Tags (1)
No ratings
Version history
Last update:
‎11-19-2025 03:16 AM
Updated by: