May I ask if the S32R294 or S32R41 chips can be used for linear frequency modulation continuous wave radar applications in other bands besides millimeter wave radar?
Hello,
The processors are not constrained like this
As long as the radar front-end device has compatible MIPI-CSI2/DPHY interface then it can be connected to S32R
Best regards,
Peter