I used the"./assemble_base_image.sh -e -b imx93 "command to create the "swu_singlecopy_rescue_imx93_emmc_20240605.sdcard" file.Upgrade the "swu_singlecopy_rescue_imx93_emmc_20240605.sdcard" file using uuu.An error has occurred.
"This wic have NOT terminate tag after"
D:\share\imx-matter_2023-q4_imx8mmevk-matter>uuu.exe -b emmc_all swu_singlecopy_rescue_imx93_emmc_20240605.sdcard
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.165-0-g7347a80
Success 0 Failure 1
2:33 1/ 1 [This wic have NOT terminate tag after ] SDPS: boot -scanterm -f swu_singlecopy_rescue_imx93_emmc_20240605
D:\share\imx-matter_2023-q4_imx8mmevk-matter>pause
请按任意键继续. . .
This reply shows you have no idea about the NXP BSP source code as a NXP engineer.
Further, the root cause is not the extension .sdcard.
In your opnion, if rename .wic to .sdcard, the image can be changed. It needs dd command.
In your mind, like a .txt file, when you rename to .mp4, it could become a movie.
Hi. @tgt007
For .sdcard you need to use dd command flash it to your SD card.
thinks!
@tgt007 I have sent you the answer and listed all the souce code for this root cause by private message.
You can decide to public it now.
I will pubilc it later to give NXP engineer chance to really read their own code, which is existing for years.
Hi @tgt007
Please use the "uuu -b emmc
If NXP engineers do not know their own code, then I can provide you with training and provide the answer to this question.
hi, @tgt007
I think this can help you:
B.R
HI, @tgt007
Where did you get this command and the shell file?
B.R
Hi, @tgt007
You should use emmc_all with .wic file. you can ru the uuu see more help about uuu.
B.R