1881151_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1881151_en-US

1881151_en-US

CAN TJA1145AT/0Z & TJA1145AT/FD/0Z Essentially different

Customer feedback they use CAN TJA1145AT/0Z & TJA1145AT/FD/0Z,It was all used according to the CAN FD function, and there were no problems。Therefore, what is the specific difference between FD and FD in model naming。There are still differences from the specifications, as shown in the figure。Thanks!

微信图片_20240605111320.png

Re: CAN TJA1145AT/0Z & TJA1145AT/FD/0Z Essentially different

Dear Louis,

please refer to the section 7.3.2 in the TJA1145A datasheet. Depending on the CFDC bit setting the  TJA1145AT and the TJA1145AT/FD will behave same (CFDC=0=>error counter increments) or (CFDC=1) the TJA1145AT/FD will ignore the CAN FD frames=>error counter decrements.

JozefKozon_0-1717569894265.png

JozefKozon_1-1717570002324.png

With Best Regards,

Jozef


标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 02:08 PM
更新人: