Hardware Configuration:
Issue Description: I have successfully implemented a simple bootloader on the QSPI internal memory, which initializes the SDRAM (32 MB), FlexSpi interface, and then jumps to the application stored in the external QSPI memory for XIP execution. This setup works correctly with a basic "hello world" application (blinking LED and console output).
However, when I attempt to run a more complex application containing extensive C++ code and utilizing the graphic controller, the system quickly encounters a hard fault from a seemingly random address. The same application works perfectly in the internal QSPI memory.
Code Used for Initialization (based on the example polling_transfer from the sdk boards/evkmimxrt1064/driver_examples/flexspi/nor/polling_transfer):
static void init_qspi_flash_on_front_panel(void)
{
SETUP(IOMUXC_GPIO_AD_B1_09_FLEXSPIA_DQS, 1, IOMUX_KEEPER_DOWN | IOMUX_SPD_MAX | IOMUX_DSE(6) | IOMUX_SLEW_FAST);
SETUP(IOMUXC_GPIO_AD_B1_10_FLEXSPIA_DATA03, 0, IOMUX_KEEPER_DOWN | IOMUX_SPD_MAX | IOMUX_DSE(6) | IOMUX_SLEW_FAST);
SETUP(IOMUXC_GPIO_AD_B1_11_FLEXSPIA_DATA02, 0, IOMUX_KEEPER_DOWN | IOMUX_SPD_MAX | IOMUX_DSE(6) | IOMUX_SLEW_FAST);
SETUP(IOMUXC_GPIO_AD_B1_12_FLEXSPIA_DATA01, 0, IOMUX_KEEPER_DOWN | IOMUX_SPD_MAX | IOMUX_DSE(6) | IOMUX_SLEW_FAST);
SETUP(IOMUXC_GPIO_AD_B1_13_FLEXSPIA_DATA00, 0, IOMUX_KEEPER_DOWN | IOMUX_SPD_MAX | IOMUX_DSE(6) | IOMUX_SLEW_FAST);
SETUP(IOMUXC_GPIO_AD_B1_14_FLEXSPIA_SCLK, 0, IOMUX_KEEPER_DOWN | IOMUX_SPD_MAX | IOMUX_DSE(6) | IOMUX_SLEW_FAST);
SETUP(IOMUXC_GPIO_AD_B1_15_FLEXSPIA_SS0_B, 0, IOMUX_KEEPER_DOWN | IOMUX_SPD_MAX | IOMUX_DSE(6) | IOMUX_SLEW_FAST);
}void init_ext_flex_spi()
{
uint32_t i = 0;
status_t status;
uint8_t vendorID = 0;
flexspi_nor_flash_init(EXAMPLE_FLEXSPI);
/* Get vendor ID. */
status = flexspi_nor_get_vendor_id(EXAMPLE_FLEXSPI, &vendorID);
if (status != kStatus_Success)
{
LOG("FAIL flexspi_nor_get_vendor_id");
Q_ASSERT(false);
}
LOG("Vendor ID: 0x%x\r\n", vendorID);
/* Enter quad mode. */
status = flexspi_nor_enable_quad_mode(EXAMPLE_FLEXSPI);
if (status != kStatus_Success)
{
LOG("FAIL flexspi_nor_enable_quad_mode");
Q_ASSERT(false);
}
}void flexspi_nor_flash_init(FLEXSPI_Type *base)
{
flexspi_config_t config;
#if defined(CACHE_MAINTAIN) && CACHE_MAINTAIN
flexspi_cache_status_t cacheStatus;
flexspi_nor_disable_cache(&cacheStatus);
#endif
flexspi_clock_init();
/*Get FLEXSPI default settings and configure the flexspi. */
FLEXSPI_GetDefaultConfig(&config);
/*Set AHB buffer size for reading data through AHB bus. */
config.ahbConfig.enableAHBPrefetch = true;
config.ahbConfig.enableAHBBufferable = true;
config.ahbConfig.enableReadAddressOpt = true;
config.ahbConfig.enableAHBCachable = true;
config.rxSampleClock = kFLEXSPI_ReadSampleClkLoopbackFromDqsPad;
FLEXSPI_Init(base, &config);
/* Configure flash settings according to serial flash feature. */
FLEXSPI_SetFlashConfig(base, &deviceconfig, FLASH_PORT);
/* Update LUT table. */
FLEXSPI_UpdateLUT(base, 0, customLUT, CUSTOM_LUT_LENGTH);
/* Do software reset. */
FLEXSPI_SoftwareReset(base);
#if defined(CACHE_MAINTAIN) && CACHE_MAINTAIN
flexspi_nor_enable_cache(cacheStatus);
#endif
}flexspi_device_config_t deviceconfig = {
.flexspiRootClk = 120000000,
.flashSize = FLASH_SIZE,
.CSIntervalUnit = kFLEXSPI_CsIntervalUnit1SckCycle,
.CSInterval = 2,
.CSHoldTime = 3,
.CSSetupTime = 3,
.dataValidTime = 0,
.columnspace = 0,
.enableWordAddress = 0,
.AWRSeqIndex = 0,
.AWRSeqNumber = 0,
.ARDSeqIndex = NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD,
.ARDSeqNumber = 1,
.AHBWriteWaitUnit = kFLEXSPI_AhbWriteWaitUnit2AhbCycle,
.AHBWriteWaitInterval = 0,
};void flexspi_clock_init()
{
const clock_usb_pll_config_t g_ccmConfigUsbPll = {.loopDivider = 0U};
CLOCK_InitUsb1Pll(&g_ccmConfigUsbPll);
CLOCK_InitUsb1Pfd(kCLOCK_Pfd0, 24);
CLOCK_SetMux(kCLOCK_FlexspiMux, 0x3); /* Choose PLL3 PFD0 clock as flexspi source clock. */
CLOCK_SetDiv(kCLOCK_FlexspiDiv, 2); /* flexspi clock 120M. */
}The FlexSpi clock is set to 120 MHz. I attempted to increase it to 132 MHz (by using PLL2_PFD2 set to 396 MHz and FlexSpi divider set to 3), but this resulted in incorrect vendor ID readings.
Request for Assistance:
Thank you for your assistance.
Michael