1877178_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1877178_en-US

1877178_en-US

MC33771C idle state

Hi, after power up (no CSB activity, I saw VCOM fixed on it) MC33771C consume 6mA. shouldn't it go to idle state?

Thanks!


Re: MC33771C idle state

Hi Alessandro,

please refer to the Figure 8. in the MC33771C full datasheet. The MC33771C can switch to Idle mode only from the INIT mode if the communication is not active. If the MC33771C is not initialized within 60s, then it switches to Idle mode. Please refer to the sections 9.3.2 and 9.3.3. From Normal mode you can send it to Sleep mode by software command. Please refer to section 9.3.4.

With Best Regards,

Jozef

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 02:21 PM
更新者: