1876413_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1876413_en-US

1876413_en-US

Getting started with FreeRTOS in S32K DS 3.5

Hi All,  New to the S32K DS and am trying to get some code working with FreeRTOS for the K344.

I am working off SW32K3_FreeRTOS_10.6.0_4.0.0_CD_D2312_ReleaseNotes. From these:

Installation flow:
1. Install S32Design Studio 3.5: S32DS.3.5_b220726_win32.x86_64.exe
2. Install Update 8 for S32DS: com.nxp.s32ds.update_3.5.8.20231116041033.zip
3. Install development package for S32K3XX: com.nxp.s32ds.s32k3xx.update_3.5.8.20231116045533.zip
4. Install development package for S32K396: SW32K39x_S32DS_3.5.6_D2309.zip
5. Install RTD updatesite: SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip


For steps 2, 3 and 4; where do I find these zip files. They do not appear to be included with the standalone "SW32K3_FreeRTOS_10.6.0_4.0.0_CD_D2312" package that I started with. I searched the forums for a while, but couldn't seem to find them.

In general what is the best way to find these update packages (there are so many).

I tried skipping ahead to just:

"Open Help -> S32DS Extensions and Updates. From the next windows,
select "FreeRTOS for S32K3XX_S32M27x" then click Install/Update"

But unsurprisingly, this fails due to a missing dependency. 

Any help is appreciated. Thanks.

Re: Getting started with FreeRTOS in S32K DS 3.5

Hi @JaGaISS 

I am attaching the links where you can download the corresponding packages. 

2 > S32 Design Studio 3.5 Update 8 D2311

3 and 4 > S32K3 Standard Software > Automotive SW - S32K3 - S32 Design Studio >  S32 Design Studio 3.5.6 RTM with support for S32K39x devices and S32 Design Studio 3.5.8 Development Package with support for S32K3xx devices. 

The zip file you will download from those links should be added to S32DS through S32DS Extensions and Updates > Add Update Sites.


B.R.

VaneB

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 02:26 PM
Updated by: