I have two CANs used in my PCB. CAN1, CAN3.
I am using message buffers for TX and RX.
#define RX_MESSAGE_BUFFER_NUM (9)
#define TX_MESSAGE_BUFFER_NUM (8)
#define USE_CANFD (0)
** I am trying to take any Classical Standard or Extended CAN message with interrupt and send it back with +1 increment for coming id and each received can data.
** I am using interrupt for only receiving. For transmitting, I do not use interrupt. I sent it with "FLEXCAN_WriteTxMb" non blocking- method.
** Even though I am sending only one time, FLEXCAN sends continously data. I disabled "loopback" disabled at init procedure. However, it behaves as I stated.
Here is my simple code important areas :
/*
#define EXAMPLE_CAN CAN1
#define EXAMPLE_FLEXCAN_IRQn CAN1_IRQn
#define EXAMPLE_FLEXCAN_IRQHandler CAN1_IRQHandler
*/
#define EXAMPLE_CAN CAN3
#define EXAMPLE_FLEXCAN_IRQn CAN3_IRQn
#define EXAMPLE_FLEXCAN_IRQHandler CAN3_IRQHandler
void EXAMPLE_FLEXCAN_IRQHandler(void){
uint64_t flag = 1U;
if (0U != FLEXCAN_GetMbStatusFlags(EXAMPLE_CAN, flag << RX_MESSAGE_BUFFER_NUM))
{
FLEXCAN_ClearMbStatusFlags(EXAMPLE_CAN, flag << RX_MESSAGE_BUFFER_NUM);
(void)FLEXCAN_ReadRxMb(EXAMPLE_CAN, RX_MESSAGE_BUFFER_NUM, &rxFrame);
rxComplete = true;
}
SDK_ISR_EXIT_BARRIER;
}
flexcan_config_t flexcanConfig;
flexcan_rx_mb_config_t mbConfig;
clock_root_config_t rootCfg = {0};
rootCfg.mux = FLEXCAN_CLOCK_SOURCE_SELECT;
rootCfg.div = FLEXCAN_CLOCK_SOURCE_DIVIDER;
/* CLOCK_SetRootClock(kCLOCK_Root_Can1, &rootCfg);*/
CLOCK_SetRootClock(kCLOCK_Root_Can3, &rootCfg);
FLEXCAN_GetDefaultConfig(&flexcanConfig);
flexcanConfig.bitRate = 250000U;
flexcanConfig.enableLoopBack = false;
FLEXCAN_Init(EXAMPLE_CAN, &flexcanConfig, EXAMPLE_CAN_CLK_FREQ);
mbConfig.format = kFLEXCAN_FrameFormatExtend;
mbConfig.type = kFLEXCAN_FrameTypeData;
mbConfig.id = FLEXCAN_ID_EXT(0x00000000);
FLEXCAN_SetRxMbConfig(EXAMPLE_CAN, RX_MESSAGE_BUFFER_NUM, &mbConfig, true);
FLEXCAN_SetTxMbConfig(EXAMPLE_CAN, TX_MESSAGE_BUFFER_NUM, true);
FLEXCAN_EnableMbInterrupts(EXAMPLE_CAN, flag << RX_MESSAGE_BUFFER_NUM);
(void)EnableIRQ(EXAMPLE_FLEXCAN_IRQn);
while (true)
{
rxComplete = false;
while (!rxComplete)
{
}
rxFrame.id = FLEXCAN_ID_EXT(rxFrame.id) + 0x01;
rxFrame.dataByte0 += 1;
rxFrame.dataByte1 += 1;
rxFrame.dataByte2 += 1;
rxFrame.dataByte3 += 1;
rxFrame.dataByte4 += 1;
rxFrame.dataByte5 += 1;
rxFrame.dataByte6 += 1;
rxFrame.dataByte7 += 1;
if (kStatus_Success == FLEXCAN_WriteTxMb(EXAMPLE_CAN, TX_MESSAGE_BUFFER_NUM, &rxFrame))
{;}
** I have one data logger with sending capability. I am also using debugger to find the problem. What I see is that; as soon as I send such as 0x18aabbcc id message, it produces continously interrupt and that is why I am taking 0x18aabbcd, 0x18aabbce, 0x18aabbcf...
** I read with debugger in interrupt handler, there is always "1" in RX_MESSAGE_BUFFER_NUM place in IFLAG register. So it continously produces interrupt. I do not understand where I am missing?
Many thanks @PetrS for your very quick response.
You are right. MCR[SRXDIS] was 0 means self reception enabled.
After your guide, I noticed that disableSelfReception flag controls SRXDIS bit. After changing it, everything now works as accepted. Thanks a lot again.
flexcanConfig.enableLoopBack = false;
flexcanConfig.disableSelfReception =true;
Hi,
exact setting is hidden here, but it seems you can have self-reception enabled. Check MCR[SRXDIS] bit.
BR, Petr
Hi @PetrS, I see the you replied most questions on FLEXCAN for MPC and S32 series. I am using IMXRT1176 but thinks flexcan structure is similiar. Can you please help me my above issue regarding CAN?
Thank you