Hello,
I am assessing a possible use of the T1013 in an application that performs access to an FPGA. My hardware/firmware friends use the EBI in 5xxx devices and the eLBC in the P1013; I would like to know if the equivalent in the T1013 would be the IFC.
As the T1023/24/13/14 states "The IFC supports both NAND and NOR flash, as well as a
general purpose memory-mapped interface for connecting low speed ASICs and FPGAs", I was wondering if "low speed" in this context means something similar to the 66MHz of a MPC5777C EBI or something much slower.
Thanks!
Ricardo
The equivalent in the T1013 is IFC.
"Low speed" in this context means something similar to the 66MHz of a MPC5777C EBI.