1870716_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1870716_en-US

1870716_en-US

Timer not working even in free running mode using PEmicro debugger

Hi team,

I am using imxrt1170 eval board and even our custom board with imxrt1176 controller.

when we connect USB debugging using the usb to micro-b cable the timer code is executing and timer is also working, but when we connect the PE micro-USB debugger to the eval board and debug, even in free running mode (without any breakpoint) also the timer code is not working.

Any pin or functionality affecting the timers of imxrt1170 eval board with the PE micro-USB debugger.

Jeevan_0-1716378852325.pngJeevan_0-1716378852325.png


Re: Timer not working even in free running mode using PEmicro debugger

Is there any same setting for systick timer also and PIT (programmable interrupt timer) using in debug mode to get enabled.

Re: Timer not working even in free running mode using PEmicro debugger

Hello @Jeevan ,

In order for your timer to continue counting in Debug mode, the bit called "DBGEN" in the register called "GPT Control Register (CR)" should be in 1. The purpose of this bit is enabled or disable the timer when the code is in debug mode, as show in the next image that was obtained in the RMHabib_Melchor_Santos_0-1716504825709.pngHabib_Melchor_Santos_0-1716504825709.png



Also, if you experience any issue, do not hesitate to let me know.

BR

Habib.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 02:36 PM
更新者: