1870611_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1870611_en-US

1870611_en-US

Unable to detect IMXRT1160 EVK with provisioning tool

Hi, is there a guide for how to connect the IMXRT1160 EVK with the secure provisioning tool (V8) as I'm getting connection failed when trying to use the USB port. I've tried both USB1 & USB2 on the EVK but get the same result. Also does a specific example program need to be run when trying to connect? 

failed connection.png

Any suggestions greatly appreciated.

Kind regards

Ian

Re: Unable to detect IMXRT1160 EVK with provisioning toolThat's great thanks for the help, it was SW1 I needed to change to 0010Re: Unable to detect IMXRT1160 EVK with provisioning tool

Hi Ian,

1. check the power supply,  J38 should be set to 3-4 for power from USB

2. check the switches to set the board to ISP mode: SW1: 0001  (to run the application, change the switch to 0010)

Here is the photo of RT1170-EVK, where the jumpers are located and where the cable should be connected. RT1160-EVK should be similar.

marektrmac_0-1716378120280.jpeg


タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 02:39 PM
更新者: