1866329_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1866329_en-US

1866329_en-US

Example_S32K344_decouple_RTD400_Ip_C40_DS35

*******************************************************************************************************
* Detailed Description:
* DCF Record decouples CM7_0 and CM_1 on S32K344
* Find first available location in UTEST.
* By default, first available address is 0x1B000768U
*
* NOTE: There is a bug in the RTD version.
* Change FLS_MAX_VIRTUAL_SECTOR to 528 in C40_Ip_Cfg.h
* ------------------------------------------------------------------------------
* Test HW: : S32K344EVB-Q257
* MCU: : S32K344
* Project : RTD AUTOSAR 4.7
* Platform : CORTEXM
* Peripheral : S32K3XX
* Dependencies : none
* Autosar Version : 4.7.0
* Autosar Revision : ASR_REL_4_7_REV_0000
* Autosar Conf.Variant :
* SW Version : 4.0.0
* Build Version : S32K3_RTD_4_0_0_P20_D2403_ASR_REL_4_7_REV_0000_20240315
*******************************************************************************************************

Re: Example_S32K344_decouple_RTD400_Ip_C40_DS35

Hello @dmitry_buchynski,

Thanks for the feedback.

It has been fixed.


Regards,

Daniel

Re: Example_S32K344_decouple_RTD400_Ip_C40_DS35_v1

Hello, @danielmartynek 
I have a few questions and notes:
1) Is it aplicable for s32k358?
2) In the main.c line 33:
     * By default, first available address is 0x1B000780U
I suppose it should be 0x1B000768U according to description

3) in the main.c lines 115 and 116:
    DCF_record[0] = 0x00000100; /* DCF Control Word */
    DCF_record[1] = 0x00100004; /* DCF Data Word, LOCKSTEP = 0 */

I think the comments are incorrect and the first one should be DCF data word and the second DCF control word

4) in the main.c line 116:
 DCF_record[1] = 0x00100004;

is the parity bit missing here and it actually must be 0x00100006 to match parity with DCF_record[0] = 0x00000100; ? 

标记 (1)
无评分
版本历史
最后更新:
‎11-19-2025 03:16 AM
更新人: