I have updated lpddr4x_timing.c and spl.c in the existing board/freescale/imx93_evk u-boot source folder to reflect custom DRAM and PMIC integrations. I was able to build the flash binary file and successfully deploy it on the eMMC storage.
Is there any guidance for creating a custom board configuration for u-boot?
I have been trying to create a separate configuration for the custom board, in the source tree, using the steps outlined below:
cp -R board/freescale/imx93_evk board/freescale/imx93_som
cp include/configs/imx93_evk.h include/configs/imx93_som.h
cp arch/arm/dts/imx93-11x11-evk.dts arch/arm/dts/imx93-11x11-som.dts
cp arch/arm/dts/imx93-11x11-evk-u-boot.dtsi arch/arm/dts/imx93-11x11-som-u-boot.dtsiUpdated board/freescale/imx93_som/Kconfig with this content:
if TARGET_IMX93_11X11_SOM
config SYS_BOARD
default "imx93_som"
config SYS_VENDOR
default "freescale"
config SYS_CONFIG_NAME
default "imx93_som"
choice
prompt "Select DDR Type"
default IMX93_EVK_LPDDR4X if TARGET_IMX93_11X11_SOM
config IMX93_EVK_LPDDR4X
bool "Using LPDDR4X Timing and PMIC voltage"
select IMX9_LPDDR4X
help
Select the LPDDR4X timing and 0.6V VDDQ
config IMX93_EVK_LPDDR4
bool "Using LPDDR4 Timing and PMIC voltage"
select IMX9_LPDDR4X
help
Select the LPDDR4 timing and 1.1V VDDQ
endchoice
endifUpdated arch/arm/mach-imx/imx9/Kconfig with the following addition:
...
config TARGET_IMX93_11X11_SOM
bool "imx93_11x11_som"
select OF_BOARD_FIXUP
select IMX93
...
source "board/freescale/imx93_som/Kconfig"
...Updated arch/arm/dts/Makefile and added an entry for a custom dts file:
dtb-$(CONFIG_ARCH_IMX9) += \
imx93-11x11-evk.dtb \
imx93-11x11-som.dtb \
imx93-14x14-evk.dtb \
imx93-9x9-qsb.dtb \
imx93-9x9-qsb-ontat-wvga-panel.dtb \
imx91p-11x11-evk.dtb \
imx91p-9x9-qsb-ontat-wvga-panel.dtb \
imx91p-9x9-qsb-spinand.dtbUpdated .config file with the following changes:
29,30c29,30
< CONFIG_SYS_BOARD="imx93_evk"
< CONFIG_SYS_CONFIG_NAME="imx93_evk"
---
> CONFIG_SYS_BOARD="imx93_som"
> CONFIG_SYS_CONFIG_NAME="imx93_som"
195c195
< CONFIG_DEFAULT_DEVICE_TREE="imx93-11x11-evk"
---
> CONFIG_DEFAULT_DEVICE_TREE="imx93-11x11-som"
202c202
< CONFIG_TARGET_IMX93_11X11_EVK=y
---
> # CONFIG_TARGET_IMX93_11X11_EVK is not set
206,207c206
< CONFIG_IMX93_EVK_LPDDR4X=y
< # CONFIG_IMX93_EVK_LPDDR4 is not set
---
> CONFIG_TARGET_IMX93_11X11_SOM=y
431c430
< CONFIG_DEFAULT_FDT_FILE="imx93-11x11-evk.dtb"
---
> CONFIG_DEFAULT_FDT_FILE="imx93-11x11-som.dtb"
936c935
< CONFIG_OF_LIST="imx93-11x11-evk"
---
> CONFIG_OF_LIST="imx93-11x11-som"
938c937
< CONFIG_SPL_OF_LIST="imx93-11x11-evk"
---
> CONFIG_SPL_OF_LIST="imx93-11x11-som"However, I get the following error when trying to make a build:
...
AR spl/fs/built-in.o
LDS spl/u-boot-spl.lds
LD spl/u-boot-spl
aarch64-poky-linux-ld.bfd: board/freescale/imx93_som/spl.o: in function `spl_dram_init':
/home/user/controls/Uboot/user-som/source/board/freescale/imx93_som/spl.c:76: undefined reference to `dram_timing'
aarch64-poky-linux-ld.bfd: /home/user/controls/Uboot/user-som/source/board/freescale/imx93_som/spl.c:76: undefined reference to `dram_timing'
make[2]: *** [/home/user/controls/Uboot/user-som/source/scripts/Makefile.spl:528: spl/u-boot-spl] Error 1
make[1]: *** [/home/user/controls/Uboot/user-som/source/Makefile:2044: spl/u-boot-spl] Error 2
make[1]: Leaving directory '/home/user/controls/Uboot/user-som/artifacts'
make: *** [Makefile:177: sub-make] Error 2
make: Leaving directory '/home/user/controls/Uboot/user-som/source'
Did I miss anything?
Any input appreciated, thanks in advance.
I would try updating some additional variables in .config file as shown below:
CONFIG_DEFAULT_DEVICE_TREE="imx93-som"
CONFIG_OF_LIST="imx93-som"
CONFIG_SPL_OF_LIST="imx93-som"
Regards
Hi @abt
I am currently stuck at the same error you got :
aarch64-poky-linux-ld.bfd: board/freescale/imx93_som/spl.o: in function `spl_dram_init':
/home/user/uboot-imx-2023.04-A1/board/freescale/imx93_som/spl.c:78:(.text.spl_dram_init+0xc): undefined reference to `dram_timing'
aarch64-poky-linux-ld.bfd: /home/user/uboot-imx-2023.04-A1/board/freescale/imx93_som/spl.c:78:(.text.spl_dram_init+0x10): undefined reference to `dram_timing'
make[1]: *** [scripts/Makefile.spl:528: spl/u-boot-spl] Error 1
I have added the missing step in red and also updated the Makefile as you have mentionned before but still stuck at the same error.
Is there any other missing step for resolving this error please ?
Here is the missing step in red:
cp -R board/freescale/imx93_evk/ board/freescale/imx93_som
mv board/freescale/imx93_som/imx93_evk.c board/freescale/imx93_som/imx93_som.c
cp include/configs/imx93_evk.h include/configs/imx93_som.h
cp arch/arm/dts/imx93-11x11-evk.dts arch/arm/dts/imx93-11x11-som.dts
cp arch/arm/dts/imx93-11x11-evk-u-boot.dtsi arch/arm/dts/imx93-11x11-som-u-boot.dtsi
I forgot to also mention these changes:
diff --git a/board/freescale/imx93_som/Makefile b/board/freescale/imx93_som/Makefile
index b6b978dd..4710b954 100644
--- a/board/freescale/imx93_som/Makefile
+++ b/board/freescale/imx93_som/Makefile
@@ -4,7 +4,7 @@
# SPDX-License-Identifier: GPL-2.0+
#
-obj-y += imx93_evk.o
+obj-y += imx93_som.o
ifdef CONFIG_SPL_BUILD
obj-y += spl.oHi @abt,
What was the missing step?
Thanks in advance.
My problem has been solved. I was missing a step.