1864911_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1864911_en-US

1864911_en-US

LPSPI SEND question.

hi.

i would like to use the send function of LPSPI0.

(LPSPI_DRV_MasterTransferBlocking)

but now there is no signal.(oscilloscope)


Attachment 1. H/W circuit diagram.

Attachment 2. config setting.

Attachment 3. code init.


i have a question here.

Is transmisson possible even with only LPSPI0_OUT?

Or should I connect another pin? (ex. LPSPI0_PCS1)


only the send function is needed.

what are the requirements for that feature?


(i using 32K146)


thank you.

Re: LPSPI SEND question.

Hi 

As the Master, you should at least initialize the Serial Clock pin.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

标记 (1)
无评分
版本历史
最后更新:
‎11-22-2025 07:35 AM
更新人: