1862817_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1862817_en-US

1862817_en-US

LPC802 dev/evk board - where can I get the example application source code ?

Hi,

I'd like to work through the source code of the example application that the LPC802 dev kit has pre-installed.

This is the app that reads the temperature sensor, potentiometer, etc and lights LED's in a face pattern.

This source code would seem to be an excellent starting point as it's interfacing with most peripherals on the board.

I have the SDK installed but it doesn't seem to contain the source code for this example app.

Internet searches refer to example bundles, but I can't find one for LPC802 dev board.

Where can I get the LPC802 dev/evk board example application source code ?

Thanks in advance.

LPC800Re: LPC802 dev/evk board - where can I get the example application source code ?Hi Hang,

Apologies for very late reply.

Thank you very much for providing this.
Re: LPC802 dev/evk board - where can I get the example application source code ?

Hi @paulw2 

The LPC802 dev/evk board example application source code is in the attachment.

Please kindly check it.

Hope this will help you.

BR

Hang

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-22-2025 07:38 AM
更新者: