I'm trying to connect a GPS 1PPS signal to a FRWY-LS1046 via a GPIO line.
I've done the following:
Kernel config:
CONFIG_PPS=y
CONFIG_PPS_CLIENT_GPIO=m
CONFIG_PPS_DEBUG=yfsl-ls1046a.dtsi:
pps {
compatible = "pps-gpio";
gpios = <&gpio3 11 0>;
assert-falling-edge;
};The kernel logs show pps1 fails to get setup:
[ 941.608348] genirq: Setting trigger mode 1 for irq 83 failed (mpc8xxx_irq_set_type+0x0/0xf8)
[ 941.616823] pps_core: unregistering pps1
[ 941.617053] pps_core: deallocating pps1
[ 941.617063] pps-gpio pps: failed to acquire IRQ 83
[ 941.621915] pps-gpio: probe of pps failed with error -22Is there a problem with using GPIO3_11 (427) for this? Is it on a GPIO expander or something?
I can read the PPS signal on the GPIO so I know I've got the correct pin.
Apologies - I had made a mistake - my .dtsi looked like this when it failed:
pps {
compatible = "pps-gpio";
gpios = <&gpio3 11 0>;
assert-rising-edge;
};This is evidently wrong - for rising edge you remove the assert-falling-edge line.
It looks like pps1 is now registered.