Hello,
Q1: I noticed that we have S32G-VNP-EVB and S32G-VNP-EVB3, assuming that they are similar and there are only some modifications in EVB3, right?
Q2: As we know that S32G-VNP-EVB includes platform board and processor board
So does that mean there are
platform board and processor board for EVB and
platform board - 3 and processor board - 3 for EVB3?
Q4: I can find the schematic of processor boards
SCH-32170_B4.pdf and S32G-PROCEVB3-S board – REV A Schematics.pdf
they should be belong to EVB and EVB3, right?
Q5: assuming that EVB3 processor board is based on EVB processor board
why in the Revision History of S32G-PROCEVB3-S board – REV A Schematics.pdf
it cannot find the history of SCH-32170_B4.pdf?
Q6: for platform board, I can only find SCH-30081_D.pdf
is it belong to EVB? where to find another version for EVB3?
Thanks
It is clear now, thank you, Daniel
Hi,
Below will be some comments on regards of your questions:
Q1: I noticed that we have S32G-VNP-EVB and S32G-VNP-EVB3, assuming that they are similar and there are only some modifications in EVB3, right?
[DA]: Don't know if we can say they are similar. They do have differences that could impact your development (i.e. there are 2 UART ports available under EVB3, while there is only 1 under EVB). We say that they are similar on regards of they both were designed for S32G platforms.
Q2: As we know that S32G-VNP-EVB includes platform board and processor board. So does that mean there are platform board and processor board for EVB and platform board - 3 and processor board - 3 for EVB3?
[DA]: We understand that the processor board is the one that relates to the EVB/EVB3 product. The platform board relates to the PLATEVB product. There is no specific PLATEVB3 product, only PLATEVB with different revisions.
Q4: I can find the schematic of processor boards SCH-32170_B4.pdf and S32G-PROCEVB3-S board – REV A Schematics.pdf they should be belong to EVB and EVB3, right?
[DA]: We understand that you are saying the following:
If so, this is correct.
Q5: assuming that EVB3 processor board is based on EVB processor board why in the Revision History of S32G-PROCEVB3-S board – REV A Schematics.pdf. it cannot find the history of SCH-32170_B4.pdf?
[DA]: It can be based, but the design is different. As of why it was not a revision for EVB, this decision seems to be related to the design team itself. It is not common to add a revision for a different board even if it shares similarities.
Q6: for platform board, I can only find SCH-30081_D.pdf is it belong to EVB? where to find another version for EVB3?
[DA]: PLATEVB does not relates to EVB or EVB3, it is a different product. For that situation, PLATEVB seems to be shared with both EVB and EVB3.
Please, let us know.